An in-memory representation of a ZigBee APS frame of an incoming or outgoing message.

Public Attributes#

uint16_t
uint16_t
uint16_t
uint8_t
uint8_t

Public Attribute Documentation#

profileId#

uint16_t sl_zigbee_aps_frame_t::profileId

The application profile ID that describes the format of the message.


Definition at line 1322 of file stack/include/sl_zigbee_types.h

clusterId#

uint16_t sl_zigbee_aps_frame_t::clusterId

The cluster ID for this message.


Definition at line 1324 of file stack/include/sl_zigbee_types.h

sourceEndpoint#

uint8_t sl_zigbee_aps_frame_t::sourceEndpoint

The source endpoint.


Definition at line 1326 of file stack/include/sl_zigbee_types.h

destinationEndpoint#

uint8_t sl_zigbee_aps_frame_t::destinationEndpoint

The destination endpoint.


Definition at line 1328 of file stack/include/sl_zigbee_types.h

options#

sl_zigbee_aps_option_t sl_zigbee_aps_frame_t::options

A bitmask of options from the enumeration above.


Definition at line 1330 of file stack/include/sl_zigbee_types.h

groupId#

uint16_t sl_zigbee_aps_frame_t::groupId

The group ID for this message, if it is multicast mode.


Definition at line 1332 of file stack/include/sl_zigbee_types.h

sequence#

uint8_t sl_zigbee_aps_frame_t::sequence

The sequence number.


Definition at line 1334 of file stack/include/sl_zigbee_types.h

radius#

uint8_t sl_zigbee_aps_frame_t::radius

Definition at line 1335 of file stack/include/sl_zigbee_types.h