This describes a one of several different types of keys and its associated data.
Public Attributes#
Public Attribute Documentation#
bitmask#
sl_zigbee_key_struct_bitmask_t sl_zigbee_key_struct_t::bitmask
This bitmask indicates whether various fields in the structure contain valid data. It also contains the index of the network the key belongs to.
key#
sl_zigbee_key_data_t sl_zigbee_key_struct_t::key
This is the actual key data. It will contain valid data based on the sl_zigbee_key_struct_bitmask_t.
psa_id#
uint32_t sl_zigbee_key_struct_t::psa_id
Internal only: the PSA ID that this key struct maps to. It will contain valid data based on the sl_zigbee_key_struct_bitmask_t.
outgoingFrameCounter#
uint32_t sl_zigbee_key_struct_t::outgoingFrameCounter
This is the outgoing frame counter associated with the key. It will contain valid data based on the sl_zigbee_key_struct_bitmask_t.
incomingFrameCounter#
uint32_t sl_zigbee_key_struct_t::incomingFrameCounter
This is the incoming frame counter associated with the key. It will contain valid data based on the sl_zigbee_key_struct_bitmask_t.
sequenceNumber#
uint8_t sl_zigbee_key_struct_t::sequenceNumber
This is the sequence number associated with the key. It will contain valid data based on the sl_zigbee_key_struct_bitmask_t.
partnerEUI64#
sl_802154_long_addr_t sl_zigbee_key_struct_t::partnerEUI64
This is the Partner EUI64 associated with the key. It will contain valid data based on the sl_zigbee_key_struct_bitmask_t.