Describe the Initial Security features and requirements that will be used when forming or joining ZigBee Light Link networks.
Public Attributes#
uint32_t
Public Attribute Documentation#
bitmask#
uint32_t sl_zigbee_zll_initial_security_state_t::bitmask
This bitmask is unused. All values are reserved for future use.
keyIndex#
sl_zigbee_zll_key_index_t sl_zigbee_zll_initial_security_state_t::keyIndex
The key encryption algorithm advertised by the application.
encryptionKey#
sl_zigbee_key_data_t sl_zigbee_zll_initial_security_state_t::encryptionKey
The encryption key for use by algorithms that require it.
preconfiguredKey#
sl_zigbee_key_data_t sl_zigbee_zll_initial_security_state_t::preconfiguredKey
The pre-configured link key used during classical ZigBee commissioning.