You are viewing documentation for version:
This is a unique identifier for referencing Zigbee Over-the-air upgrade images. It is used by the OTA plugins when passing around information about an upgrade file. 
Public Attribute Documentation#
manufacturerId#
uint16_t sl_zigbee_af_ota_image_id_t::manufacturerId
imageTypeId#
uint16_t sl_zigbee_af_ota_image_id_t::imageTypeId
firmwareVersion#
uint32_t sl_zigbee_af_ota_image_id_t::firmwareVersion
deviceSpecificFileEui64#
uint8_t sl_zigbee_af_ota_image_id_t::deviceSpecificFileEui64[EUI64_SIZE]
This is only used for device-specific files. It will be set to all zeroes when the image does not have an upgrade destination field in it. Little endian format.