Bootloader#
EmberZNet bootload API.
See bootload.h for source code.
Functions#
Transmit the given bootload message to a neighboring node using a specific 802.15.4 header that allows the EmberZNet stack and the Ember bootloader to recognize the message but will not interfere with other Zigbee stacks.
Invoked by the EmberZNet stack when a bootload message is received. If the application includes sl_zigbee_incoming_bootload_message_handler(), it must define SL_ZIGBEE_APPLICATION_HAS_BOOTLOAD_HANDLERS in its CONFIGURATION_HEADER.
Invoked by the EmberZNet stack when the MAC has finished transmitting a bootload message. If the application includes this callback, it must define SL_ZIGBEE_APPLICATION_HAS_BOOTLOAD_HANDLERS in its CONFIGURATION_HEADER.
Function Documentation#
sl_zigbee_send_bootload_message#
sl_status_t sl_zigbee_send_bootload_message (bool broadcast, sl_802154_long_addr_t destEui64, uint8_t messageLength, uint8_t * messageContents)
Transmit the given bootload message to a neighboring node using a specific 802.15.4 header that allows the EmberZNet stack and the Ember bootloader to recognize the message but will not interfere with other Zigbee stacks.
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| bool | N/A | broadcast | If true, the destination address and PAN ID are both set to the broadcast address.  | 
| sl_802154_long_addr_t | N/A | destEui64 | The EUI64 of the target node. Ignored if the broadcast field is set to true.  | 
| uint8_t | N/A | messageLength | Length of the message to be sent.  | 
| uint8_t * | N/A | messageContents | The bootloader message to send.  | 
Returns
::SL_STATUS_OK if the message was successfully submitted to the transmit queue, and ::SL_STATUS_FAIL otherwise.
sl_zigbee_incoming_bootload_message_handler#
void sl_zigbee_incoming_bootload_message_handler (sl_802154_long_addr_t longId, sl_zigbee_rx_packet_info_t * packetInfo, uint8_t messageLength, uint8_t * messageContents)
Invoked by the EmberZNet stack when a bootload message is received. If the application includes sl_zigbee_incoming_bootload_message_handler(), it must define SL_ZIGBEE_APPLICATION_HAS_BOOTLOAD_HANDLERS in its CONFIGURATION_HEADER.
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| sl_802154_long_addr_t | N/A | longId | The EUI64 of the sending node.  | 
| sl_zigbee_rx_packet_info_t * | N/A | packetInfo | Information about the incoming packet.  | 
| uint8_t | N/A | messageLength | Length of the bootload message that was sent.  | 
| uint8_t * | N/A | messageContents | The bootload message that was sent.  | 
sl_zigbee_bootload_transmit_complete_handler#
void sl_zigbee_bootload_transmit_complete_handler (sl_status_t status, uint8_t messageLength, uint8_t * messageContents)
Invoked by the EmberZNet stack when the MAC has finished transmitting a bootload message. If the application includes this callback, it must define SL_ZIGBEE_APPLICATION_HAS_BOOTLOAD_HANDLERS in its CONFIGURATION_HEADER.
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| sl_status_t | N/A | status | ::SL_STATUS_OK if the transmission was successful, or ::SL_STATUS_ZIGBEE_DELIVERY_FAILED if not.  | 
| uint8_t | N/A | messageLength | Length of the message that was sent.  | 
| uint8_t * | N/A | messageContents | The message that was sent.  |