/*******************************************************************************
* @file
* @brief SL Status Codes.
*******************************************************************************
* # License
* <b>Copyright 2019 Silicon Laboratories Inc. www.silabs.com</b>
*******************************************************************************
*
* SPDX-License-Identifier: Zlib
*
* The licensor of this software is Silicon Laboratories Inc.
*
* This software is provided 'as-is', without any express or implied
* warranty. In no event will the authors be held liable for any damages
* arising from the use of this software.
*
* Permission is granted to anyone to use this software for any purpose,
* including commercial applications, and to alter it and redistribute it
* freely, subject to the following restrictions:
*
* 1. The origin of this software must not be misrepresented; you must not
* claim that you wrote the original software. If you use this software
* in a product, an acknowledgment in the product documentation would be
* appreciated but is not required.
* 2. Altered source versions must be plainly marked as such, and must not be
* misrepresented as being the original software.
* 3. This notice may not be removed or altered from any source distribution.
*
******************************************************************************/
#ifndef SL_STATUS_H
#define SL_STATUS_H
#include <stdint.h>
/*******************************************************************************
* @addtogroup status Status Codes
* @details Status Codes contains error and status code definitions used by
* Simplicity SDK software components and stacks. This module also
* provides routines to read the string linked with the error and
* status codes.
* @{
******************************************************************************/
// -----------------------------------------------------------------------------
// Space Defines
#define SL_STATUS_SPACE_MASK ((sl_status_t)0xFF00)
#define SL_STATUS_GENERIC_SPACE ((sl_status_t)0x0000)
#define SL_STATUS_PLATFORM_1_SPACE ((sl_status_t)0x0100)
#define SL_STATUS_PLATFORM_2_SPACE ((sl_status_t)0x0200)
#define SL_STATUS_HARDWARE_SPACE ((sl_status_t)0x0300)
#define SL_STATUS_BLUETOOTH_SPACE ((sl_status_t)0x0400)
#define SL_STATUS_BLUETOOTH_MESH_SPACE ((sl_status_t)0x0500)
#define SL_STATUS_CAN_CANOPEN_SPACE ((sl_status_t)0x0600)
#define SL_STATUS_CONNECT_SPACE ((sl_status_t)0x0700)
#define SL_STATUS_NET_SUITE_SPACE ((sl_status_t)0x0800)
#define SL_STATUS_THREAD_SPACE ((sl_status_t)0x0900)
#define SL_STATUS_USB_SPACE ((sl_status_t)0x0A00)
#define SL_STATUS_WIFI_SPACE ((sl_status_t)0x0B00)
#define SL_STATUS_ZIGBEE_SPACE ((sl_status_t)0x0C00)
#define SL_STATUS_Z_WAVE_SPACE ((sl_status_t)0x0D00)
#define SL_STATUS_GECKO_OS_1_SPACE ((sl_status_t)0x0E00)
#define SL_STATUS_GECKO_OS_2_SPACE ((sl_status_t)0x0F00)
#define SL_STATUS_BLUETOOTH_CTRL_SPACE ((sl_status_t)0x1000)
#define SL_STATUS_BLUETOOTH_ATT_SPACE ((sl_status_t)0x1100)
#define SL_STATUS_BLUETOOTH_SMP_SPACE ((sl_status_t)0x1200)
#define SL_STATUS_BLUETOOTH_MESH_FOUNDATION_SPACE ((sl_status_t)0x1300)
#define SL_STATUS_WISUN_SPACE ((sl_status_t)0x1400)
#define SL_STATUS_COMPUTE_SPACE ((sl_status_t)0x1500)
// -----------------------------------------------------------------------------
// Status Defines
// -----------------------------------------------------------------------------
// Generic Errors
#define SL_STATUS_OK ((sl_status_t)0x0000)
#define SL_STATUS_FAIL ((sl_status_t)0x0001)
// State Errors
#define SL_STATUS_INVALID_STATE ((sl_status_t)0x0002)
#define SL_STATUS_NOT_READY ((sl_status_t)0x0003)
#define SL_STATUS_BUSY ((sl_status_t)0x0004)
#define SL_STATUS_IN_PROGRESS ((sl_status_t)0x0005)
#define SL_STATUS_ABORT ((sl_status_t)0x0006)
#define SL_STATUS_TIMEOUT ((sl_status_t)0x0007)
#define SL_STATUS_PERMISSION ((sl_status_t)0x0008)
#define SL_STATUS_WOULD_BLOCK ((sl_status_t)0x0009)
#define SL_STATUS_IDLE ((sl_status_t)0x000A)
#define SL_STATUS_IS_WAITING ((sl_status_t)0x000B)
#define SL_STATUS_NONE_WAITING ((sl_status_t)0x000C)
#define SL_STATUS_SUSPENDED ((sl_status_t)0x000D)
#define SL_STATUS_NOT_AVAILABLE ((sl_status_t)0x000E)
#define SL_STATUS_NOT_SUPPORTED ((sl_status_t)0x000F)
#define SL_STATUS_INITIALIZATION ((sl_status_t)0x0010)
#define SL_STATUS_NOT_INITIALIZED ((sl_status_t)0x0011)
#define SL_STATUS_ALREADY_INITIALIZED ((sl_status_t)0x0012)
#define SL_STATUS_DELETED ((sl_status_t)0x0013)
#define SL_STATUS_ISR ((sl_status_t)0x0014)
#define SL_STATUS_NETWORK_UP ((sl_status_t)0x0015)
#define SL_STATUS_NETWORK_DOWN ((sl_status_t)0x0016)
#define SL_STATUS_NOT_JOINED ((sl_status_t)0x0017)
#define SL_STATUS_NO_BEACONS ((sl_status_t)0x0018)
// Allocation/ownership Errors
#define SL_STATUS_ALLOCATION_FAILED ((sl_status_t)0x0019)
#define SL_STATUS_NO_MORE_RESOURCE ((sl_status_t)0x001A)
#define SL_STATUS_EMPTY ((sl_status_t)0x001B)
#define SL_STATUS_FULL ((sl_status_t)0x001C)
#define SL_STATUS_WOULD_OVERFLOW ((sl_status_t)0x001D)
#define SL_STATUS_HAS_OVERFLOWED ((sl_status_t)0x001E)
#define SL_STATUS_OWNERSHIP ((sl_status_t)0x001F)
#define SL_STATUS_IS_OWNER ((sl_status_t)0x0020)
// Invalid Parameters Errors
#define SL_STATUS_INVALID_PARAMETER ((sl_status_t)0x0021)
#define SL_STATUS_NULL_POINTER ((sl_status_t)0x0022)
#define SL_STATUS_INVALID_CONFIGURATION ((sl_status_t)0x0023)
#define SL_STATUS_INVALID_MODE ((sl_status_t)0x0024)
#define SL_STATUS_INVALID_HANDLE ((sl_status_t)0x0025)
#define SL_STATUS_INVALID_TYPE ((sl_status_t)0x0026)
#define SL_STATUS_INVALID_INDEX ((sl_status_t)0x0027)
#define SL_STATUS_INVALID_RANGE ((sl_status_t)0x0028)
#define SL_STATUS_INVALID_KEY ((sl_status_t)0x0029)
#define SL_STATUS_INVALID_CREDENTIALS ((sl_status_t)0x002A)
#define SL_STATUS_INVALID_COUNT ((sl_status_t)0x002B)
#define SL_STATUS_INVALID_SIGNATURE ((sl_status_t)0x002C)
#define SL_STATUS_NOT_FOUND ((sl_status_t)0x002D)
#define SL_STATUS_ALREADY_EXISTS ((sl_status_t)0x002E)
// IO/Communication Errors
#define SL_STATUS_IO ((sl_status_t)0x002F)
#define SL_STATUS_IO_TIMEOUT ((sl_status_t)0x0030)
#define SL_STATUS_TRANSMIT ((sl_status_t)0x0031)
#define SL_STATUS_TRANSMIT_UNDERFLOW ((sl_status_t)0x0032)
#define SL_STATUS_TRANSMIT_INCOMPLETE ((sl_status_t)0x0033)
#define SL_STATUS_TRANSMIT_BUSY ((sl_status_t)0x0034)
#define SL_STATUS_RECEIVE ((sl_status_t)0x0035)
#define SL_STATUS_OBJECT_READ ((sl_status_t)0x0036)
#define SL_STATUS_OBJECT_WRITE ((sl_status_t)0x0037)
#define SL_STATUS_MESSAGE_TOO_LONG ((sl_status_t)0x0038)
// EEPROM/Flash Errors
#define SL_STATUS_EEPROM_MFG_VERSION_MISMATCH ((sl_status_t)0x0039)
#define SL_STATUS_EEPROM_STACK_VERSION_MISMATCH ((sl_status_t)0x003A)
#define SL_STATUS_FLASH_WRITE_INHIBITED ((sl_status_t)0x003B)
#define SL_STATUS_FLASH_VERIFY_FAILED ((sl_status_t)0x003C)
#define SL_STATUS_FLASH_PROGRAM_FAILED ((sl_status_t)0x003D)
#define SL_STATUS_FLASH_ERASE_FAILED ((sl_status_t)0x003E)
// MAC Errors
#define SL_STATUS_MAC_NO_DATA ((sl_status_t)0x003F)
#define SL_STATUS_MAC_NO_ACK_RECEIVED ((sl_status_t)0x0040)
#define SL_STATUS_MAC_INDIRECT_TIMEOUT ((sl_status_t)0x0041)
#define SL_STATUS_MAC_UNKNOWN_HEADER_TYPE ((sl_status_t)0x0042)
#define SL_STATUS_MAC_ACK_HEADER_TYPE ((sl_status_t)0x0043)
#define SL_STATUS_MAC_COMMAND_TRANSMIT_FAILURE ((sl_status_t)0x0044)
// CLI_STORAGE Errors
#define SL_STATUS_CLI_STORAGE_NVM_OPEN_ERROR ((sl_status_t)0x0045)
// Security status codes
#define SL_STATUS_SECURITY_IMAGE_CHECKSUM_ERROR ((sl_status_t)0x0046)
#define SL_STATUS_SECURITY_DECRYPT_ERROR ((sl_status_t)0x0047)
// Command status codes
#define SL_STATUS_COMMAND_IS_INVALID ((sl_status_t)0x0048)
#define SL_STATUS_COMMAND_TOO_LONG ((sl_status_t)0x0049)
#define SL_STATUS_COMMAND_INCOMPLETE ((sl_status_t)0x004A)
// Misc Errors
#define SL_STATUS_BUS_ERROR ((sl_status_t)0x004B)
// Unified MAC Errors
#define SL_STATUS_CCA_FAILURE ((sl_status_t)0x004C)
// Scan errors
#define SL_STATUS_MAC_SCANNING ((sl_status_t)0x004D)
#define SL_STATUS_MAC_INCORRECT_SCAN_TYPE ((sl_status_t)0x004E)
#define SL_STATUS_INVALID_CHANNEL_MASK ((sl_status_t)0x004F)
#define SL_STATUS_BAD_SCAN_DURATION ((sl_status_t)0x0050)
// MAC transmit related status
#define SL_STATUS_MAC_TRANSMIT_QUEUE_FULL ((sl_status_t)0x0053)
#define SL_STATUS_TRANSMIT_SCHEDULER_FAIL ((sl_status_t)0x0054)
#define SL_STATUS_TRANSMIT_INVALID_CHANNEL ((sl_status_t)0x0055)
#define SL_STATUS_TRANSMIT_INVALID_POWER ((sl_status_t)0x0056)
#define SL_STATUS_TRANSMIT_ACK_RECEIVED ((sl_status_t)0x0057)
#define SL_STATUS_TRANSMIT_BLOCKED ((sl_status_t)0x0058)
// NVM3 specific errors
#define SL_STATUS_NVM3_ALIGNMENT_INVALID ((sl_status_t)0x0059)
#define SL_STATUS_NVM3_SIZE_TOO_SMALL ((sl_status_t)0x005A)
#define SL_STATUS_NVM3_PAGE_SIZE_NOT_SUPPORTED ((sl_status_t)0x005B)
#define SL_STATUS_NVM3_TOKEN_INIT_FAILED ((sl_status_t)0x005C)
#define SL_STATUS_NVM3_OPENED_WITH_OTHER_PARAMETERS ((sl_status_t)0x005D)
#define SL_STATUS_NVM3_NO_VALID_PAGES ((sl_status_t)0x005E)
#define SL_STATUS_NVM3_OBJECT_SIZE_NOT_SUPPORTED ((sl_status_t)0x005F)
#define SL_STATUS_NVM3_OBJECT_IS_NOT_DATA ((sl_status_t)0x0060)
#define SL_STATUS_NVM3_OBJECT_IS_NOT_A_COUNTER ((sl_status_t)0x0061)
#define SL_STATUS_NVM3_WRITE_DATA_SIZE ((sl_status_t)0x0062)
#define SL_STATUS_NVM3_READ_DATA_SIZE ((sl_status_t)0x0063)
#define SL_STATUS_NVM3_INIT_WITH_FULL_NVM ((sl_status_t)0x0064)
#define SL_STATUS_NVM3_RESIZE_PARAMETER ((sl_status_t)0x0065)
#define SL_STATUS_NVM3_RESIZE_NOT_ENOUGH_SPACE ((sl_status_t)0x0066)
#define SL_STATUS_NVM3_ERASE_COUNT_ERROR ((sl_status_t)0x0067)
#define SL_STATUS_NVM3_NVM_ACCESS ((sl_status_t)0x0068)
#define SL_STATUS_NVM3_WRITE_TO_NOT_ERASED ((sl_status_t)0x006D)
#define SL_STATUS_NVM3_INVALID_ADDR ((sl_status_t)0x006E)
#define SL_STATUS_NVM3_KEY_MISMATCH ((sl_status_t)0x006F)
#define SL_STATUS_NVM3_SIZE_ERROR ((sl_status_t)0x0070)
#define SL_STATUS_NVM3_EMULATOR ((sl_status_t)0x0071)
// Security status codes
#define SL_STATUS_SECURITY_ENCRYPT_ERROR ((sl_status_t)0x0072)
#define SL_STATUS_SECURITY_KEY_ERROR ((sl_status_t)0x0073)
#define SL_STATUS_SECURITY_RANDOM_NUM_GEN_ERROR ((sl_status_t)0x0074)
// Bluetooth status codes
#define SL_STATUS_BT_OUT_OF_BONDS ((sl_status_t)0x0402)
#define SL_STATUS_BT_UNSPECIFIED ((sl_status_t)0x0403)
#define SL_STATUS_BT_HARDWARE ((sl_status_t)0x0404)
#define SL_STATUS_BT_NO_BONDING ((sl_status_t)0x0406)
#define SL_STATUS_BT_CRYPTO ((sl_status_t)0x0407)
#define SL_STATUS_BT_DATA_CORRUPTED ((sl_status_t)0x0408)
#define SL_STATUS_BT_INVALID_SYNC_HANDLE ((sl_status_t)0x040A)
#define SL_STATUS_BT_INVALID_MODULE_ACTION ((sl_status_t)0x040B)
#define SL_STATUS_BT_RADIO ((sl_status_t)0x040C)
#define SL_STATUS_BT_L2CAP_REMOTE_DISCONNECTED ((sl_status_t)0x040D)
#define SL_STATUS_BT_L2CAP_LOCAL_DISCONNECTED ((sl_status_t)0x040E)
#define SL_STATUS_BT_L2CAP_CID_NOT_EXIST ((sl_status_t)0x040F)
#define SL_STATUS_BT_L2CAP_LE_DISCONNECTED ((sl_status_t)0x0410)
#define SL_STATUS_BT_L2CAP_FLOW_CONTROL_VIOLATED ((sl_status_t)0x0412)
#define SL_STATUS_BT_L2CAP_FLOW_CONTROL_CREDIT_OVERFLOWED ((sl_status_t)0x0413)
#define SL_STATUS_BT_L2CAP_NO_FLOW_CONTROL_CREDIT ((sl_status_t)0x0414)
#define SL_STATUS_BT_L2CAP_CONNECTION_REQUEST_TIMEOUT ((sl_status_t)0x0415)
#define SL_STATUS_BT_L2CAP_INVALID_CID ((sl_status_t)0x0416)
#define SL_STATUS_BT_L2CAP_WRONG_STATE ((sl_status_t)0x0417)
#define SL_STATUS_BT_PS_STORE_FULL ((sl_status_t)0x041B)
#define SL_STATUS_BT_PS_KEY_NOT_FOUND ((sl_status_t)0x041C)
#define SL_STATUS_BT_APPLICATION_MISMATCHED_OR_INSUFFICIENT_SECURITY ((sl_status_t)0x041D)
#define SL_STATUS_BT_APPLICATION_ENCRYPTION_DECRYPTION_ERROR ((sl_status_t)0x041E)
// Bluetooth controller status codes
#define SL_STATUS_BT_CTRL_UNKNOWN_CONNECTION_IDENTIFIER ((sl_status_t)0x1002)
#define SL_STATUS_BT_CTRL_AUTHENTICATION_FAILURE ((sl_status_t)0x1005)
#define SL_STATUS_BT_CTRL_PIN_OR_KEY_MISSING ((sl_status_t)0x1006)
#define SL_STATUS_BT_CTRL_MEMORY_CAPACITY_EXCEEDED ((sl_status_t)0x1007)
#define SL_STATUS_BT_CTRL_CONNECTION_TIMEOUT ((sl_status_t)0x1008)
#define SL_STATUS_BT_CTRL_CONNECTION_LIMIT_EXCEEDED ((sl_status_t)0x1009)
#define SL_STATUS_BT_CTRL_SYNCHRONOUS_CONNECTION_LIMIT_EXCEEDED ((sl_status_t)0x100A)
#define SL_STATUS_BT_CTRL_ACL_CONNECTION_ALREADY_EXISTS ((sl_status_t)0x100B)
#define SL_STATUS_BT_CTRL_COMMAND_DISALLOWED ((sl_status_t)0x100C)
#define SL_STATUS_BT_CTRL_CONNECTION_REJECTED_DUE_TO_LIMITED_RESOURCES ((sl_status_t)0x100D)
#define SL_STATUS_BT_CTRL_CONNECTION_REJECTED_DUE_TO_SECURITY_REASONS ((sl_status_t)0x100E)
#define SL_STATUS_BT_CTRL_CONNECTION_REJECTED_DUE_TO_UNACCEPTABLE_BD_ADDR ((sl_status_t)0x100F)
#define SL_STATUS_BT_CTRL_CONNECTION_ACCEPT_TIMEOUT_EXCEEDED ((sl_status_t)0x1010)
#define SL_STATUS_BT_CTRL_UNSUPPORTED_FEATURE_OR_PARAMETER_VALUE ((sl_status_t)0x1011)
#define SL_STATUS_BT_CTRL_INVALID_COMMAND_PARAMETERS ((sl_status_t)0x1012)
#define SL_STATUS_BT_CTRL_REMOTE_USER_TERMINATED ((sl_status_t)0x1013)
#define SL_STATUS_BT_CTRL_REMOTE_DEVICE_TERMINATED_CONNECTION_DUE_TO_LOW_RESOURCES ((sl_status_t)0x1014)
#define SL_STATUS_BT_CTRL_REMOTE_POWERING_OFF ((sl_status_t)0x1015)
#define SL_STATUS_BT_CTRL_CONNECTION_TERMINATED_BY_LOCAL_HOST ((sl_status_t)0x1016)
#define SL_STATUS_BT_CTRL_REPEATED_ATTEMPTS ((sl_status_t)0x1017)
#define SL_STATUS_BT_CTRL_PAIRING_NOT_ALLOWED ((sl_status_t)0x1018)
#define SL_STATUS_BT_CTRL_UNSUPPORTED_REMOTE_FEATURE ((sl_status_t)0x101A)
#define SL_STATUS_BT_CTRL_INVALID_LL_PARAMETERS ((sl_status_t)0x101E)
#define SL_STATUS_BT_CTRL_UNSPECIFIED_ERROR ((sl_status_t)0x101F)
#define SL_STATUS_BT_CTRL_LL_RESPONSE_TIMEOUT ((sl_status_t)0x1022)
#define SL_STATUS_BT_CTRL_LL_PROCEDURE_COLLISION ((sl_status_t)0x1023)
#define SL_STATUS_BT_CTRL_ENCRYPTION_MODE_NOT_ACCEPTABLE ((sl_status_t)0x1025)
#define SL_STATUS_BT_CTRL_LINK_KEY_CANNOT_BE_CHANGED ((sl_status_t)0x1026)
#define SL_STATUS_BT_CTRL_INSTANT_PASSED ((sl_status_t)0x1028)
#define SL_STATUS_BT_CTRL_PAIRING_WITH_UNIT_KEY_NOT_SUPPORTED ((sl_status_t)0x1029)
#define SL_STATUS_BT_CTRL_DIFFERENT_TRANSACTION_COLLISION ((sl_status_t)0x102A)
#define SL_STATUS_BT_CTRL_CHANNEL_ASSESSMENT_NOT_SUPPORTED ((sl_status_t)0x102E)
#define SL_STATUS_BT_CTRL_INSUFFICIENT_SECURITY ((sl_status_t)0x102F)
#define SL_STATUS_BT_CTRL_PARAMETER_OUT_OF_MANDATORY_RANGE ((sl_status_t)0x1030)
#define SL_STATUS_BT_CTRL_SIMPLE_PAIRING_NOT_SUPPORTED_BY_HOST ((sl_status_t)0x1037)
#define SL_STATUS_BT_CTRL_HOST_BUSY_PAIRING ((sl_status_t)0x1038)
#define SL_STATUS_BT_CTRL_CONNECTION_REJECTED_DUE_TO_NO_SUITABLE_CHANNEL_FOUND ((sl_status_t)0x1039)
#define SL_STATUS_BT_CTRL_CONTROLLER_BUSY ((sl_status_t)0x103A)
#define SL_STATUS_BT_CTRL_UNACCEPTABLE_CONNECTION_INTERVAL ((sl_status_t)0x103B)
#define SL_STATUS_BT_CTRL_ADVERTISING_TIMEOUT ((sl_status_t)0x103C)
#define SL_STATUS_BT_CTRL_CONNECTION_TERMINATED_DUE_TO_MIC_FAILURE ((sl_status_t)0x103D)
#define SL_STATUS_BT_CTRL_CONNECTION_FAILED_TO_BE_ESTABLISHED ((sl_status_t)0x103E)
#define SL_STATUS_BT_CTRL_MAC_CONNECTION_FAILED ((sl_status_t)0x103F)
#define SL_STATUS_BT_CTRL_COARSE_CLOCK_ADJUSTMENT_REJECTED_BUT_WILL_TRY_TO_ADJUST_USING_CLOCK_DRAGGING ((sl_status_t)0x1040)
#define SL_STATUS_BT_CTRL_UNKNOWN_ADVERTISING_IDENTIFIER ((sl_status_t)0x1042)
#define SL_STATUS_BT_CTRL_LIMIT_REACHED ((sl_status_t)0x1043)
#define SL_STATUS_BT_CTRL_OPERATION_CANCELLED_BY_HOST ((sl_status_t)0x1044)
#define SL_STATUS_BT_CTRL_PACKET_TOO_LONG ((sl_status_t)0x1045)
#define SL_STATUS_BT_CTRL_TOO_LATE ((sl_status_t)0x1046)
#define SL_STATUS_BT_CTRL_TOO_EARLY ((sl_status_t)0x1047)
#define SL_STATUS_BT_CTRL_INSUFFICIENT_CHANNELS ((sl_status_t)0x1048)
// Bluetooth attribute status codes
#define SL_STATUS_BT_ATT_INVALID_HANDLE ((sl_status_t)0x1101)
#define SL_STATUS_BT_ATT_READ_NOT_PERMITTED ((sl_status_t)0x1102)
#define SL_STATUS_BT_ATT_WRITE_NOT_PERMITTED ((sl_status_t)0x1103)
#define SL_STATUS_BT_ATT_INVALID_PDU ((sl_status_t)0x1104)
#define SL_STATUS_BT_ATT_INSUFFICIENT_AUTHENTICATION ((sl_status_t)0x1105)
#define SL_STATUS_BT_ATT_REQUEST_NOT_SUPPORTED ((sl_status_t)0x1106)
#define SL_STATUS_BT_ATT_INVALID_OFFSET ((sl_status_t)0x1107)
#define SL_STATUS_BT_ATT_INSUFFICIENT_AUTHORIZATION ((sl_status_t)0x1108)
#define SL_STATUS_BT_ATT_PREPARE_QUEUE_FULL ((sl_status_t)0x1109)
#define SL_STATUS_BT_ATT_ATT_NOT_FOUND ((sl_status_t)0x110A)
#define SL_STATUS_BT_ATT_ATT_NOT_LONG ((sl_status_t)0x110B)
#define SL_STATUS_BT_ATT_INSUFFICIENT_ENC_KEY_SIZE ((sl_status_t)0x110C)
#define SL_STATUS_BT_ATT_INVALID_ATT_LENGTH ((sl_status_t)0x110D)
#define SL_STATUS_BT_ATT_UNLIKELY_ERROR ((sl_status_t)0x110E)
#define SL_STATUS_BT_ATT_INSUFFICIENT_ENCRYPTION ((sl_status_t)0x110F)
#define SL_STATUS_BT_ATT_UNSUPPORTED_GROUP_TYPE ((sl_status_t)0x1110)
#define SL_STATUS_BT_ATT_INSUFFICIENT_RESOURCES ((sl_status_t)0x1111)
#define SL_STATUS_BT_ATT_OUT_OF_SYNC ((sl_status_t)0x1112)
#define SL_STATUS_BT_ATT_VALUE_NOT_ALLOWED ((sl_status_t)0x1113)
#define SL_STATUS_BT_ATT_APPLICATION ((sl_status_t)0x1180)
#define SL_STATUS_BT_ATT_WRITE_REQUEST_REJECTED ((sl_status_t)0x11FC)
#define SL_STATUS_BT_ATT_CLIENT_CHARACTERISTIC_CONFIGURATION_DESCRIPTOR_IMPROPERLY_CONFIGURED ((sl_status_t)0x11FD)
#define SL_STATUS_BT_ATT_PROCEDURE_ALREADY_IN_PROGRESS ((sl_status_t)0x11FE)
#define SL_STATUS_BT_ATT_OUT_OF_RANGE ((sl_status_t)0x11FF)
// Bluetooth Security Manager Protocol status codes
#define SL_STATUS_BT_SMP_PASSKEY_ENTRY_FAILED ((sl_status_t)0x1201)
#define SL_STATUS_BT_SMP_OOB_NOT_AVAILABLE ((sl_status_t)0x1202)
#define SL_STATUS_BT_SMP_AUTHENTICATION_REQUIREMENTS ((sl_status_t)0x1203)
#define SL_STATUS_BT_SMP_CONFIRM_VALUE_FAILED ((sl_status_t)0x1204)
#define SL_STATUS_BT_SMP_PAIRING_NOT_SUPPORTED ((sl_status_t)0x1205)
#define SL_STATUS_BT_SMP_ENCRYPTION_KEY_SIZE ((sl_status_t)0x1206)
#define SL_STATUS_BT_SMP_COMMAND_NOT_SUPPORTED ((sl_status_t)0x1207)
#define SL_STATUS_BT_SMP_UNSPECIFIED_REASON ((sl_status_t)0x1208)
#define SL_STATUS_BT_SMP_REPEATED_ATTEMPTS ((sl_status_t)0x1209)
#define SL_STATUS_BT_SMP_INVALID_PARAMETERS ((sl_status_t)0x120A)
#define SL_STATUS_BT_SMP_DHKEY_CHECK_FAILED ((sl_status_t)0x120B)
#define SL_STATUS_BT_SMP_NUMERIC_COMPARISON_FAILED ((sl_status_t)0x120C)
#define SL_STATUS_BT_SMP_BREDR_PAIRING_IN_PROGRESS ((sl_status_t)0x120D)
#define SL_STATUS_BT_SMP_CROSS_TRANSPORT_KEY_DERIVATION_GENERATION_NOT_ALLOWED ((sl_status_t)0x120E)
#define SL_STATUS_BT_SMP_KEY_REJECTED ((sl_status_t)0x120F)
// Bluetooth Mesh status codes
#define SL_STATUS_BT_MESH_ALREADY_EXISTS ((sl_status_t)0x0501)
#define SL_STATUS_BT_MESH_DOES_NOT_EXIST ((sl_status_t)0x0502)
#define SL_STATUS_BT_MESH_LIMIT_REACHED ((sl_status_t)0x0503)
#define SL_STATUS_BT_MESH_INVALID_ADDRESS ((sl_status_t)0x0504)
#define SL_STATUS_BT_MESH_MALFORMED_DATA ((sl_status_t)0x0505)
#define SL_STATUS_BT_MESH_ALREADY_INITIALIZED ((sl_status_t)0x0506)
#define SL_STATUS_BT_MESH_NOT_INITIALIZED ((sl_status_t)0x0507)
#define SL_STATUS_BT_MESH_NO_FRIEND_OFFER ((sl_status_t)0x0508)
#define SL_STATUS_BT_MESH_PROV_LINK_CLOSED ((sl_status_t)0x0509)
#define SL_STATUS_BT_MESH_PROV_INVALID_PDU ((sl_status_t)0x050A)
#define SL_STATUS_BT_MESH_PROV_INVALID_PDU_FORMAT ((sl_status_t)0x050B)
#define SL_STATUS_BT_MESH_PROV_UNEXPECTED_PDU ((sl_status_t)0x050C)
#define SL_STATUS_BT_MESH_PROV_CONFIRMATION_FAILED ((sl_status_t)0x050D)
#define SL_STATUS_BT_MESH_PROV_OUT_OF_RESOURCES ((sl_status_t)0x050E)
#define SL_STATUS_BT_MESH_PROV_DECRYPTION_FAILED ((sl_status_t)0x050F)
#define SL_STATUS_BT_MESH_PROV_UNEXPECTED_ERROR ((sl_status_t)0x0510)
#define SL_STATUS_BT_MESH_PROV_CANNOT_ASSIGN_ADDR ((sl_status_t)0x0511)
#define SL_STATUS_BT_MESH_ADDRESS_TEMPORARILY_UNAVAILABLE ((sl_status_t)0x0512)
#define SL_STATUS_BT_MESH_ADDRESS_ALREADY_USED ((sl_status_t)0x0513)
#define SL_STATUS_BT_MESH_PUBLISH_NOT_CONFIGURED ((sl_status_t)0x0514)
#define SL_STATUS_BT_MESH_APP_KEY_NOT_BOUND ((sl_status_t)0x0515)
// Bluetooth Mesh foundation status codes
#define SL_STATUS_BT_MESH_FOUNDATION_INVALID_ADDRESS ((sl_status_t)0x1301)
#define SL_STATUS_BT_MESH_FOUNDATION_INVALID_MODEL ((sl_status_t)0x1302)
#define SL_STATUS_BT_MESH_FOUNDATION_INVALID_APP_KEY ((sl_status_t)0x1303)
#define SL_STATUS_BT_MESH_FOUNDATION_INVALID_NET_KEY ((sl_status_t)0x1304)
#define SL_STATUS_BT_MESH_FOUNDATION_INSUFFICIENT_RESOURCES ((sl_status_t)0x1305)
#define SL_STATUS_BT_MESH_FOUNDATION_KEY_INDEX_EXISTS ((sl_status_t)0x1306)
#define SL_STATUS_BT_MESH_FOUNDATION_INVALID_PUBLISH_PARAMS ((sl_status_t)0x1307)
#define SL_STATUS_BT_MESH_FOUNDATION_NOT_SUBSCRIBE_MODEL ((sl_status_t)0x1308)
#define SL_STATUS_BT_MESH_FOUNDATION_STORAGE_FAILURE ((sl_status_t)0x1309)
#define SL_STATUS_BT_MESH_FOUNDATION_NOT_SUPPORTED ((sl_status_t)0x130A)
#define SL_STATUS_BT_MESH_FOUNDATION_CANNOT_UPDATE ((sl_status_t)0x130B)
#define SL_STATUS_BT_MESH_FOUNDATION_CANNOT_REMOVE ((sl_status_t)0x130C)
#define SL_STATUS_BT_MESH_FOUNDATION_CANNOT_BIND ((sl_status_t)0x130D)
#define SL_STATUS_BT_MESH_FOUNDATION_TEMPORARILY_UNABLE ((sl_status_t)0x130E)
#define SL_STATUS_BT_MESH_FOUNDATION_CANNOT_SET ((sl_status_t)0x130F)
#define SL_STATUS_BT_MESH_FOUNDATION_UNSPECIFIED ((sl_status_t)0x1310)
#define SL_STATUS_BT_MESH_FOUNDATION_INVALID_BINDING ((sl_status_t)0x1311)
// -----------------------------------------------------------------------------
// Wi-Fi Errors
#define SL_STATUS_WIFI_INVALID_KEY ((sl_status_t)0x0B01)
#define SL_STATUS_WIFI_FIRMWARE_DOWNLOAD_TIMEOUT ((sl_status_t)0x0B02)
#define SL_STATUS_WIFI_UNSUPPORTED_MESSAGE_ID ((sl_status_t)0x0B03)
#define SL_STATUS_WIFI_WARNING ((sl_status_t)0x0B04)
#define SL_STATUS_WIFI_NO_PACKET_TO_RECEIVE ((sl_status_t)0x0B05)
#define SL_STATUS_WIFI_SLEEP_GRANTED ((sl_status_t)0x0B08)
#define SL_STATUS_WIFI_SLEEP_NOT_GRANTED ((sl_status_t)0x0B09)
#define SL_STATUS_WIFI_SECURE_LINK_MAC_KEY_ERROR ((sl_status_t)0x0B10)
#define SL_STATUS_WIFI_SECURE_LINK_MAC_KEY_ALREADY_BURNED ((sl_status_t)0x0B11)
#define SL_STATUS_WIFI_SECURE_LINK_RAM_MODE_NOT_ALLOWED ((sl_status_t)0x0B12)
#define SL_STATUS_WIFI_SECURE_LINK_FAILED_UNKNOWN_MODE ((sl_status_t)0x0B13)
#define SL_STATUS_WIFI_SECURE_LINK_EXCHANGE_FAILED ((sl_status_t)0x0B14)
#define SL_STATUS_WIFI_WRONG_STATE ((sl_status_t)0x0B18)
#define SL_STATUS_WIFI_CHANNEL_NOT_ALLOWED ((sl_status_t)0x0B19)
#define SL_STATUS_WIFI_NO_MATCHING_AP ((sl_status_t)0x0B1A)
#define SL_STATUS_WIFI_CONNECTION_ABORTED ((sl_status_t)0x0B1B)
#define SL_STATUS_WIFI_CONNECTION_TIMEOUT ((sl_status_t)0x0B1C)
#define SL_STATUS_WIFI_CONNECTION_REJECTED_BY_AP ((sl_status_t)0x0B1D)
#define SL_STATUS_WIFI_CONNECTION_AUTH_FAILURE ((sl_status_t)0x0B1E)
#define SL_STATUS_WIFI_RETRY_EXCEEDED ((sl_status_t)0x0B1F)
#define SL_STATUS_WIFI_TX_LIFETIME_EXCEEDED ((sl_status_t)0x0B20)
// -----------------------------------------------------------------------------
// MVP Driver and MVP Math status codes
#define SL_STATUS_COMPUTE_DRIVER_FAULT ((sl_status_t)0x1501)
#define SL_STATUS_COMPUTE_DRIVER_ALU_NAN ((sl_status_t)0x1502)
#define SL_STATUS_COMPUTE_DRIVER_ALU_OVERFLOW ((sl_status_t)0x1503)
#define SL_STATUS_COMPUTE_DRIVER_ALU_UNDERFLOW ((sl_status_t)0x1504)
#define SL_STATUS_COMPUTE_DRIVER_STORE_CONVERSION_OVERFLOW ((sl_status_t)0x1505)
#define SL_STATUS_COMPUTE_DRIVER_STORE_CONVERSION_UNDERFLOW ((sl_status_t)0x1506)
#define SL_STATUS_COMPUTE_DRIVER_STORE_CONVERSION_INFINITY ((sl_status_t)0x1507)
#define SL_STATUS_COMPUTE_DRIVER_STORE_CONVERSION_NAN ((sl_status_t)0x1508)
#define SL_STATUS_COMPUTE_MATH_NAN ((sl_status_t)0x1512)
#define SL_STATUS_COMPUTE_MATH_INFINITY ((sl_status_t)0x1513)
#define SL_STATUS_COMPUTE_MATH_OVERFLOW ((sl_status_t)0x1514)
#define SL_STATUS_COMPUTE_MATH_UNDERFLOW ((sl_status_t)0x1515)
// Zigbee status codes
#define SL_STATUS_ZIGBEE_PACKET_HANDOFF_DROPPED ((sl_status_t)0x0C01)
#define SL_STATUS_ZIGBEE_DELIVERY_FAILED ((sl_status_t)0x0C02)
#define SL_STATUS_ZIGBEE_MAX_MESSAGE_LIMIT_REACHED ((sl_status_t)0x0C03)
#define SL_STATUS_ZIGBEE_BINDING_IS_ACTIVE ((sl_status_t)0x0C04)
#define SL_STATUS_ZIGBEE_ADDRESS_TABLE_ENTRY_IS_ACTIVE ((sl_status_t)0x0C05)
#define SL_STATUS_ZIGBEE_MOVE_FAILED ((sl_status_t)0x0C06)
#define SL_STATUS_ZIGBEE_NODE_ID_CHANGED ((sl_status_t)0x0C07)
#define SL_STATUS_ZIGBEE_INVALID_SECURITY_LEVEL ((sl_status_t)0x0C08)
#define SL_STATUS_ZIGBEE_IEEE_ADDRESS_DISCOVERY_IN_PROGRESS ((sl_status_t)0x0C09)
#define SL_STATUS_ZIGBEE_APS_ENCRYPTION_ERROR ((sl_status_t)0x0C0A)
#define SL_STATUS_ZIGBEE_SECURITY_STATE_NOT_SET ((sl_status_t)0x0C0B)
#define SL_STATUS_ZIGBEE_TOO_SOON_FOR_SWITCH_KEY ((sl_status_t)0x0C0C)
#define SL_STATUS_ZIGBEE_SIGNATURE_VERIFY_FAILURE ((sl_status_t)0x0C0D)
#define SL_STATUS_ZIGBEE_KEY_NOT_AUTHORIZED ((sl_status_t)0x0C0E)
#define SL_STATUS_ZIGBEE_BINDING_HAS_CHANGED ((sl_status_t)0x0C0F)
#define SL_STATUS_ZIGBEE_TRUST_CENTER_SWAP_EUI_HAS_CHANGED ((sl_status_t)0x0C10)
#define SL_STATUS_ZIGBEE_TRUST_CENTER_SWAP_EUI_HAS_NOT_CHANGED ((sl_status_t)0x0C11)
#define SL_STATUS_ZIGBEE_INSUFFICIENT_RANDOM_DATA ((sl_status_t)0x0C12)
#define SL_STATUS_ZIGBEE_SOURCE_ROUTE_FAILURE ((sl_status_t)0x0C13)
#define SL_STATUS_ZIGBEE_MANY_TO_ONE_ROUTE_FAILURE ((sl_status_t)0x0C14)
#define SL_STATUS_ZIGBEE_STACK_AND_HARDWARE_MISMATCH ((sl_status_t)0x0C15)
#define SL_STATUS_ZIGBEE_PAN_ID_CHANGED ((sl_status_t)0x0C16)
#define SL_STATUS_ZIGBEE_CHANNEL_CHANGED ((sl_status_t)0x0C17)
#define SL_STATUS_ZIGBEE_NETWORK_OPENED ((sl_status_t)0x0C18)
#define SL_STATUS_ZIGBEE_NETWORK_CLOSED ((sl_status_t)0x0C19)
#define SL_STATUS_ZIGBEE_RECEIVED_KEY_IN_THE_CLEAR ((sl_status_t)0x0C1A)
#define SL_STATUS_ZIGBEE_NO_NETWORK_KEY_RECEIVED ((sl_status_t)0x0C1B)
#define SL_STATUS_ZIGBEE_NO_LINK_KEY_RECEIVED ((sl_status_t)0x0C1C)
#define SL_STATUS_ZIGBEE_PRECONFIGURED_KEY_REQUIRED ((sl_status_t)0x0C1D)
#define SL_STATUS_ZIGBEE_EZSP_ERROR ((sl_status_t)0x0C1E)
#define SL_STATUS_ZIGBEE_ID_DISCOVERY_FAILED ((sl_status_t)0x0C1F)
#define SL_STATUS_ZIGBEE_NO_APS_ACK ((sl_status_t)0x0C20)
#define SL_STATUS_ZIGBEE_APS_MESSAGE_CANCELED ((sl_status_t)0x0C21)
#define SL_STATUS_ZIGBEE_ID_DISCOVERY_NOT_ENABLED ((sl_status_t)0x0C22)
#define SL_STATUS_ZIGBEE_ID_DISCOVERY_UNDERWAY ((sl_status_t)0x0C23)
#define SL_STATUS_ZIGBEE_SEND_UNICAST_ROUTE_DISCOVERY_UNDERWAY ((sl_status_t)0x0C24)
#define SL_STATUS_ZIGBEE_SEND_UNICAST_FAILURE ((sl_status_t)0x0C25)
#define SL_STATUS_ZIGBEE_SEND_UNICAST_NO_ROUTE ((sl_status_t)0x0C26)
#define SL_STATUS_ZIGBEE_BROADCAST_TO_SLEEPY_CHILDREN_TIMEOUT ((sl_status_t)0x0C27)
#define SL_STATUS_ZIGBEE_BROADCAST_RELAY_FAILED ((sl_status_t)0x0C28)
// -----------------------------------------------------------------------------
// Data Types
typedef uint32_t sl_status_t;
// -----------------------------------------------------------------------------
// Functions
#ifdef __cplusplus
extern "C" {
#endif
/********************************************************************************************************
* sl_status_get_string_n()
*
* @brief Get a copy of the status string associated to the status code passed, up to
* 'buffer_length' length, if the string associated to the status code is enabled. If not,
* the error code number, in hex, prefixed by "SL_STATUS_" will be copied in the buffer
* instead.
* For example, the buffer would either contain "SL_STATUS_FAIL" if that status string is
* enabled, or "SL_STATUS_0x0001" if the string is disabled, as SL_STATUS_FAIL's
* value is 0x0001.
*
* @param status The status code from which to obtain the status string.
*
* @param buffer Pointer to a buffer in which the status string will be copied. A terminating
* null-character will be appended after the copied status string.
*
* @param buffer_length Maximum number of characters that can be written in the buffer, including the
* terminating null-character. If the status string would be longer than the
* available length, it will be truncated and a null-terminating character will
* be the last character contained in the buffer.
*
* @return The number of characters that would have been written if the buffer_length had been
* sufficiently large, not counting the terminating null character.
* If the status code is invalid, 0 or a negative number is returned.
* Notice that only when this returned value is strictly positive and less than
* buffer_length, the status string has been completely written in the buffer.
*******************************************************************************************************/
int32_t sl_status_get_string_n(sl_status_t status, char *buffer, uint32_t buffer_length);
/********************************************************************************************************
* sl_status_print()
*
* @brief Print, through printf, the string associated to the passed status code. If the string
* associated to the status code is enabled, the status string will be printed, for example
* "SL_STATUS_OK". If the string associated to the status code is disabled, the status number,
* in hex, prefixed by "SL_STATUS_" will be printed instead, for example "SL_STATUS_0x0000",
* as SL_STATUS_OK's value is 0x0000.
*
* @param status The status code of which to print the status string.
*******************************************************************************************************/
void sl_status_print(sl_status_t status);
#ifdef __cplusplus
}
#endif
#endif /* SL_STATUS_H */
Macros#
sl status space mask.
sl status generic space.
sl status platform 1 space.
sl status platform 2 space.
sl status hardware space.
sl status bluetooth space.
sl status bluetooth mesh space.
sl status can canopen space.
sl status connect space.
sl status net suite space.
sl status thread space.
sl status usb space.
sl status wifi space.
sl status zigbee space.
sl status z wave space.
sl status gecko os 1 space.
sl status gecko os 2 space.
sl status bluetooth ctrl space.
sl status bluetooth att space.
sl status bluetooth mesh foundation space.
sl status bluetooth mesh foundation space.
sl status wisun space.
sl status compute space.
No error.
Generic error.
Generic invalid state error.
Module is not ready for requested operation.
Module is busy and cannot carry out requested operation.
Operation is in progress and not yet complete (pass or fail).
Operation aborted.
Operation timed out.
Operation not allowed per permissions.
Non-blocking operation would block.
Operation/module is Idle, cannot carry requested operation.
Operation cannot be done while construct is waiting.
No task/construct waiting/pending for that action/event.
Operation cannot be done while construct is suspended.
Feature not available due to software configuration.
Feature not supported.
Initialization failed.
Module has not been initialized.
Module has already been initialized.
Object/construct has been deleted.
Illegal call from ISR.
Illegal call because network is up.
Illegal call because network is down.
Failure due to not being joined in a network.
Invalid operation as there are no beacons.
Generic allocation error.
No more resource available to perform the operation.
Item/list/queue is empty.
Item/list/queue is full.
Item would overflow.
Item/list/queue has been overflowed.
Generic ownership error.
Already/still owning resource.
Generic invalid argument or consequence of invalid argument.
Invalid null pointer received as argument.
Invalid configuration provided.
Invalid mode.
Invalid handle.
Invalid type for operation.
Invalid index.
Invalid range.
Invalid key.
Invalid credentials.
Invalid count.
Invalid signature / verification failed.
Item could not be found.
Item already exists.
Generic I/O failure.
I/O failure due to timeout.
Generic transmission error.
Transmit underflowed.
Transmit is incomplete.
Transmit is busy.
Generic reception error.
Failed to read on/via given object.
Failed to write on/via given object.
Message is too long.
EEPROM MFG version mismatch.
EEPROM Stack version mismatch.
Flash write is inhibited.
Flash verification failed.
Flash programming failed.
Flash erase failed.
MAC no data.
MAC no ACK received.
MAC indirect timeout.
MAC unknown header type.
MAC ACK unknown header type.
MAC command transmit failure.
Error in open NVM.
Image checksum is not valid.
Decryption failed.
Command was not recognized.
Command or parameter maximum length exceeded.
Data received does not form a complete command.
Bus error, e.g. invalid DMA address.
CCA failure.
MAC scanning.
MAC incorrect scan type.
Invalid channel mask.
Bad scan duration.
The MAC transmit queue is full.
The transmit attempt failed because the radio scheduler could not find a slot to transmit this packet in or a higher priority event interrupted it.
An unsupported channel setting was specified.
An unsupported power setting was specified.
The expected ACK was received after the last transmission.
The transmit attempt was blocked from going over the air. Typically this is due to the Radio Hold Off (RHO) or Coexistence plugins as they can prevent transmits based on external signals.
The initialization was aborted as the NVM3 instance is not aligned properly in memory.
The initialization was aborted as the size of the NVM3 instance is too small.
The initialization was aborted as the NVM3 page size is not supported.
The application that there was an error initializing some of the tokens.
The initialization was aborted as the NVM3 instance was already opened with other parameters.
Initialization aborted, no valid page found.
The object size is not supported.
Trying to access a data object which is currently a counter object.
Trying to access a counter object which is currently a data object.
The object is too large.
Trying to read with a length different from actual object size.
The module was opened with a full NVM.
Illegal parameter.
Not enough NVM to complete resize.
Erase counts are not valid.
A NVM function call was failing.
Write to memory that is not erased.
Invalid NVM address.
Key validation failure.
Size mismatch error.
Emulator error.
Encryption failed.
Error in obtaining crypto key.
Error in obtaining random number.
Bonding procedure can't be started because device has no space left for bond.
Unspecified error.
Hardware failure.
The bonding does not exist.
Error using crypto functions.
Data was corrupted.
Invalid periodic advertising sync handle.
Bluetooth cannot be used on this hardware.
Error received from radio.
Returned when remote disconnects the connection-oriented channel by sending disconnection request.
Returned when local host disconnect the connection-oriented channel by sending disconnection request.
Returned when local host did not find a connection-oriented channel with given destination CID.
Returned when connection-oriented channel disconnected due to LE connection is dropped.
Returned when connection-oriented channel disconnected due to remote end send data even without credit.
Returned when connection-oriented channel disconnected due to remote end send flow control credits exceed 65535.
Returned when connection-oriented channel has run out of flow control credit and local application still trying to send data.
Returned when connection-oriented channel has not received connection response message within maximum timeout.
Returned when local host received a connection-oriented channel connection response with an invalid destination CID.
Returned when local host application tries to send a command which is not suitable for L2CAP channel's current state.
Flash reserved for PS store is full.
PS key not found.
Mismatched or insufficient security level.
Encryption/decryption operation failed.
Connection does not exist, or connection open request was cancelled.
Pairing or authentication failed due to incorrect results in the pairing or authentication procedure. This could be due to an incorrect PIN or Link Key.
Pairing failed because of missing PIN, or authentication failed because of missing Key.
Controller is out of memory.
Link supervision timeout has expired.
Controller is at limit of connections it can support.
The Synchronous Connection Limit to a Device Exceeded error code indicates that the Controller has reached the limit to the number of synchronous connections that can be achieved to a device.
The ACL Connection Already Exists error code indicates that an attempt to create a new ACL Connection to a device when there is already a connection to this device.
Command requested cannot be executed because the Controller is in a state where it cannot process this command at this time.
The Connection Rejected Due To Limited Resources error code indicates that an incoming connection was rejected due to limited resources.
The Connection Rejected Due To Security Reasons error code indicates that a connection was rejected due to security requirements not being fulfilled, like authentication or pairing.
The Connection was rejected because this device does not accept the BD_ADDR. This may be because the device will only accept connections from specific BD_ADDRs.
The Connection Accept Timeout has been exceeded for this connection attempt.
A feature or parameter value in the HCI command is not supported.
Command contained invalid parameters.
User on the remote device terminated the connection.
The remote device terminated the connection because of low resources.
Remote Device Terminated Connection due to Power Off.
Local device terminated the connection.
The Controller is disallowing an authentication or pairing procedure because too little time has elapsed since the last authentication or pairing attempt failed.
The device does not allow pairing. This can be for example, when a device only allows pairing during a certain time window after some user input allows pairing.
The remote device does not support the feature associated with the issued command.
Indicates that some LMP PDU / LL Control PDU parameters were invalid.
No other error code specified is appropriate to use.
Connection terminated due to link-layer procedure timeout.
LL procedure has collided with the same transaction or procedure that is already in progress.
The requested encryption mode is not acceptable at this time.
Link key cannot be changed because a fixed unit key is being used.
LMP PDU or LL PDU that includes an instant cannot be performed because the instant when this would have occurred has passed.
It was not possible to pair as a unit key was requested and it is not supported.
LMP transaction was started that collides with an ongoing transaction.
The Controller cannot perform channel assessment because it is not supported.
The HCI command or LMP PDU sent is only possible on an encrypted link.
A parameter value requested is outside the mandatory range of parameters for the given HCI command or LMP PDU.
The IO capabilities request or response was rejected because the sending Host does not support Secure Simple Pairing even though the receiving Link Manager does.
The Host is busy with another pairing operation and unable to support the requested pairing. The receiving device should retry pairing again later.
The Controller could not calculate an appropriate value for the Channel selection operation.
Operation was rejected because the controller is busy and unable to process the request.
Remote device terminated the connection because of an unacceptable connection interval.
Advertising for a fixed duration completed or, for directed advertising, that advertising completed without a connection being created.
Connection was terminated because the Message Integrity Check (MIC) failed on a received packet.
LL initiated a connection but the connection has failed to be established. Controller did not receive any packets from remote end.
The MAC of the 802.11 AMP was requested to connect to a peer, but the connection failed.
The master, at this time, is unable to make a coarse adjustment to the piconet clock, using the supplied parameters. Instead the master will attempt to move the clock using clock dragging.
A command was sent from the Host that should identify an Advertising or Sync handle, but the Advertising or Sync handle does not exist.
Number of operations requested has been reached and has indicated the completion of the activity (e.g., advertising or scanning).
A request to the Controller issued by the Host and still pending was successfully canceled.
An attempt was made to send or receive a packet that exceeds the maximum allowed packet length.
Information was provided too late to the controller.
Information was provided too early to the controller.
Indicates that the result of the requested operation would yield too few physical channels.
The attribute handle given was not valid on this server.
The attribute cannot be read.
The attribute cannot be written.
The attribute PDU was invalid.
The attribute requires authentication before it can be read or written.
Attribute Server does not support the request received from the client.
Offset specified was past the end of the attribute.
The attribute requires authorization before it can be read or written.
Too many prepare writes have been queued.
No attribute found within the given attribute handle range.
The attribute cannot be read or written using the Read Blob Request.
The Encryption Key Size used for encrypting this link is insufficient.
The attribute value length is invalid for the operation.
The attribute request that was requested has encountered an error that was unlikely, and therefore could not be completed as requested.
The attribute requires encryption before it can be read or written.
The attribute type is not a supported grouping attribute as defined by a higher layer specification.
Insufficient Resources to complete the request.
The server requests the client to rediscover the database.
The attribute parameter value was not allowed.
When this is returned in a BGAPI response, the application tried to read or write the value of a user attribute from the GATT database.
The requested write operation cannot be fulfilled for reasons other than permissions.
The Client Characteristic Configuration descriptor is not configured according to the requirements of the profile or service.
The profile or service request cannot be serviced because an operation that has been previously triggered is still in progress.
The attribute value is out of range as defined by a profile or service specification.
The user input of passkey failed, for example, the user cancelled the operation.
Out of Band data is not available for authentication.
The pairing procedure cannot be performed as authentication requirements cannot be met due to IO capabilities of one or both devices.
The confirm value does not match the calculated compare value.
Pairing is not supported by the device.
The resultant encryption key size is insufficient for the security requirements of this device.
The SMP command received is not supported on this device.
Pairing failed due to an unspecified reason.
Pairing or authentication procedure is disallowed because too little time has elapsed since last pairing request or security request.
The Invalid Parameters error code indicates: the command length is invalid or a parameter is outside of the specified range.
Indicates to the remote device that the DHKey Check value received doesn't match the one calculated by the local device.
Indicates that the confirm values in the numeric comparison protocol do not match.
Indicates that the pairing over the LE transport failed due to a Pairing Request sent over the BR/EDR transport in process.
Indicates that the BR/EDR Link Key generated on the BR/EDR transport cannot be used to derive and distribute keys for the LE transport.
Indicates that the device chose not to accept a distributed key.
Returned when trying to add a key or some other unique resource with an ID which already exists.
Returned when trying to manipulate a key or some other resource with an ID which does not exist.
Returned when an operation cannot be executed because a pre-configured limit for keys, key bindings, elements, models, virtual addresses, provisioned devices, or provisioning sessions is reached.
Returned when trying to use a reserved address or add a "pre-provisioned" device using an address already used by some other device.
In a BGAPI response, the user supplied malformed data; in a BGAPI event, the remote end responded with malformed or unrecognized data.
An attempt was made to initialize a subsystem that was already initialized.
An attempt was made to use a subsystem that wasn't initialized yet. Call the subsystem's init function first.
Returned when trying to establish a friendship as a Low Power Node, but no acceptable friend offer message was received.
Provisioning link was unexpectedly closed before provisioning was complete.
An unrecognized provisioning PDU was received.
A provisioning PDU with wrong length or containing field values that are out of bounds was received.
An unexpected (out of sequence) provisioning PDU was received.
The computed confirmation value did not match the expected value.
Provisioning could not be continued due to insufficient resources.
The provisioning data block could not be decrypted.
An unexpected error happened during provisioning.
Device could not assign unicast addresses to all of its elements.
Returned when trying to reuse an address of a previously deleted device before an IV Index Update has been executed.
Returned when trying to assign an address that is used by one of the devices in the Device Database, or by the Provisioner itself.
Application key or publish address are not set.
Application key is not bound to a model.
Returned when address in request was not valid.
Returned when model identified is not found for a given element.
Returned when the key identified by AppKeyIndex is not stored in the node.
Returned when the key identified by NetKeyIndex is not stored in the node.
Returned when The node cannot serve the request due to insufficient resources.
Returned when the key identified is already stored in the node and the new NetKey value is different.
Returned when the model does not support the publish mechanism.
Returned when the model does not support the subscribe mechanism.
Returned when storing of the requested parameters failed.
Returned when requested setting is not supported.
Returned when the requested update operation cannot be performed due to general constraints.
Returned when the requested delete operation cannot be performed due to general constraints.
Returned when the requested bind operation cannot be performed due to general constraints.
Returned when The node cannot start advertising with Node Identity or Proxy since the maximum number of parallel advertising is reached.
Returned when the requested state cannot be set.
Returned when an unspecified error took place.
Returned when the NetKeyIndex and AppKeyIndex combination is not valid for a Config AppKey Update.
Invalid firmware keyset.
The firmware download took too long.
Unknown request ID or wrong interface ID used.
The request is successful but some parameters have been ignored.
No Packets waiting to be received.
The sleep mode is granted.
The WFx does not go back to sleep.
The SecureLink MAC key was not found.
The SecureLink MAC key is already installed in OTP.
The SecureLink MAC key cannot be installed in RAM.
The SecureLink MAC key installation failed.
SecureLink key (re)negotiation failed.
The device is in an inappropriate state to perform the request.
The request failed due to regulatory limitations.
The connection request failed because no suitable AP was found.
The connection request was aborted by host.
The connection request failed because of a timeout.
The connection request failed because the AP rejected the device.
The connection request failed because the WPA handshake did not complete successfully.
The request failed because the retry limit was exceeded.
The request failed because the MSDU life time was exceeded.
Critical fault.
ALU operation output NaN.
ALU numeric overflow.
ALU numeric underflow.
Overflow during array store.
Underflow during array store conversion.
Infinity encountered during array store conversion.
NaN encountered during array store conversion.
MATH NaN encountered.
MATH Infinity encountered.
MATH numeric overflow.
MATH numeric underflow.
Packet is dropped by packet-handoff callbacks.
The APS layer attempted to send or deliver a message and failed.
The maximum number of in-flight messages ::EMBER_APS_UNICAST_MESSAGE_COUNT has been reached.
The application is trying to delete or overwrite a binding that is in use.
The application is trying to overwrite an address table entry that is in use.
After moving, a mobile node's attempt to re-establish contact with the network failed.
The local node ID has changed. The application can get the new node ID by calling ::sl_zigbee_get_node_id()
The chosen security level is not supported by the stack.
An error occurred when trying to encrypt at the APS Level.
An error occurred when trying to encrypt at the APS Level.
There was an attempt to form or join a network with security without calling ::sl_zigbee_set_initial_security_state() first.
There was an attempt to broadcast a key switch too quickly after broadcasting the next network key. The Trust Center must wait at least a period equal to the broadcast timeout so that all routers have a chance to receive the broadcast of the new network key.
The received signature corresponding to the message that was passed to the CBKE Library failed verification and is not valid.
The message could not be sent because the link key corresponding to the destination is not authorized for use in APS data messages.
The application tried to use a binding that has been remotely modified and the change has not yet been reported to the application.
The EUI of the Trust center has changed due to a successful rejoin after TC Swapout.
A Trust Center Swapout Rejoin has occurred without the EUI of the TC changing.
An attempt to generate random bytes failed because of insufficient random data from the radio.
A Zigbee route error command frame was received indicating that a source routed message from this node failed en route.
A Zigbee route error command frame was received indicating that a message sent to this node along a many-to-one route failed en route.
A critical and fatal error indicating that the version of the stack trying to run does not match with the chip it's running on.
The local PAN ID has changed. The application can get the new PAN ID by calling ::emberGetPanId()
The channel has changed.
The network has been opened for joining.
The network has been closed for joining.
An attempt was made to join a Secured Network using a pre-configured key, but the Trust Center sent back a Network Key in-the-clear when an encrypted Network Key was required. (::EMBER_REQUIRE_ENCRYPTED_KEY)
An attempt was made to join a Secured Network, but the device did not receive a Network Key.
After a device joined a Secured Network, a Link Key was requested (::EMBER_GET_LINK_KEY_WHEN_JOINING) but no response was ever received.
An attempt was made to join a Secured Network without a pre-configured key, but the Trust Center sent encrypted data using a pre-configured key.
A Zigbee EZSP error has occured. Track the origin and corresponding EzspStatus for more info.
Node ID discovery failed.
Message was sent but no APS ACK received.
APS message was canceled.
Node ID discovery not enabled.
Message was not sent, Node ID discovery is underway.
The message was not sent because a route discovery is currently underway. There is no route to the target until the route discovery completes.
Radius is 0 or message has been dropped because route request failed or failed to submit message to tx queue.
No active route to the destination.
Broadcast message timeout while waiting for sleepy children to poll.
Expected a neighbor to relay the message, but none did.
Typedefs#
define global status variable.
Functions#
Function Documentation#
sl_status_get_string_n#
int32_t sl_status_get_string_n (sl_status_t status, char * buffer, uint32_t buffer_length)
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sl_status_t | N/A | status | |
| char * | N/A | buffer | |
| uint32_t | N/A | buffer_length |
sl_status_print#
void sl_status_print (sl_status_t status)
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sl_status_t | N/A | status |