A structure containing the information of a token.

Public Attributes#

uint32_t
bool
bool
uint32_t
uint8_t

Public Attribute Documentation#

nvm3Key#

uint32_t sl_zigbee_token_info_t::nvm3Key

NVM3 token key.


isCnt#

bool sl_zigbee_token_info_t::isCnt

The token is a counter token type.


isIdx#

bool sl_zigbee_token_info_t::isIdx

The token is an indexed token type.


size#

uint32_t sl_zigbee_token_info_t::size

Size of the object of the token.


arraySize#

uint8_t sl_zigbee_token_info_t::arraySize

The array size for the token when it is an indexed token.