You are viewing documentation for version:9.1.1PDFGP Tx queue entry. Public Attributes#boolinUsebooluseCcasl_zigbee_gp_address_taddruint8_tgpdCommandIduint8_tgpepHandleuint16_tqueueEntryLifetimeMsPublic Attribute Documentation#inUse#bool sl_zigbee_gp_tx_queue_entry_t::inUseThe entry in use useCca#bool sl_zigbee_gp_tx_queue_entry_t::useCcaUse CCA during transmit addr#sl_zigbee_gp_address_t sl_zigbee_gp_tx_queue_entry_t::addrGP address gpdCommandId#uint8_t sl_zigbee_gp_tx_queue_entry_t::gpdCommandIdGPD Command ID gpepHandle#uint8_t sl_zigbee_gp_tx_queue_entry_t::gpepHandleHandle for the outgoing message queueEntryLifetimeMs#uint16_t sl_zigbee_gp_tx_queue_entry_t::queueEntryLifetimeMsLife time in milliseconds for the entry to expire, 0 indicates no expiry