See Debugging Utilities for documentation.
License#
Copyright 2018 Silicon Laboratories Inc. www.silabs.com
The licensor of this software is Silicon Laboratories Inc. Your use of this software is governed by the terms of Silicon Labs Master Software License Agreement (MSLA) available at www.silabs.com/about-us/legal/master-software-license-agreement. This software is distributed to you in Source Code format and is governed by the sections of the MSLA applicable to Source Code.
/***************************************************************************/
#ifndef SILABS_EMBER_DEBUG_H
#define SILABS_EMBER_DEBUG_H
// Define the values for DEBUG_LEVEL
#define NO_DEBUG 0
#define BASIC_DEBUG 1
#define FULL_DEBUG 2
#define sl_zigbee_debug_init(port) do {} while (false)
#if (defined(DEBUG_LEVEL) && defined(BASIC_DEBUG) && (DEBUG_LEVEL >= BASIC_DEBUG)) || defined(DOXYGEN_SHOULD_SKIP_THIS) || !defined(SL_ZIGBEE_SCRIPTED_TEST)
#define DEBUG_ROUTINES_PRESENT
void sl_zigbee_debug_assert(const char * filename, int linenumber);
void sl_zigbee_debug_memory_dump(uint8_t *start, uint8_t *end);
void sl_zigbee_debug_binary_printf(const char * formatString, ...);
void sli_util_debug_send_vuart_message(uint8_t *buff, uint8_t len);
//#if (DEBUG_LEVEL == FULL_DEBUG) || defined(DOXYGEN_SHOULD_SKIP_THIS)
void sl_zigbee_debug_error(sl_status_t code);
bool sl_zigbee_debug_report_off(void);
void sl_zigbee_debug_report_restore(bool state);
// Format: Same as sli_legacy_serial_printf
// sl_zigbee_debug_printf("format string"[, parameters ...])
void sl_zigbee_debug_printf(const char * formatString, ...) __attribute__((format(printf, 1, 2)));
#else // (DEBUG_LEVEL >= BASIC_DEBUG) || defined(DOXYGEN_SHOULD_SKIP_THIS) || !defined(SL_ZIGBEE_SCRIPTED_TEST)
#define sl_zigbee_debug_assert(filename, linenumber) do {} while (false)
#define sl_zigbee_debug_memory_dump(start, end) do {} while (false)
#define sl_zigbee_debug_binary_printf(formatstring, ...) do {} while (false)
#define sli_util_debug_send_vuart_message(buff, len) do {} while (false)
#define sl_zigbee_debug_error(code) do {} while (false)
// Note the following doesn't have a do{}while(false)
// because it has a return value
#define sl_zigbee_debug_report_off() (false)
#define sl_zigbee_debug_report_restore(state) do {} while (false)
#define sl_zigbee_debug_printf(...) do {} while (false)
#endif // (defined(DEBUG_LEVEL) && defined(BASIC_DEBUG) && (DEBUG_LEVEL >= BASIC_DEBUG)) || defined(DOXYGEN_SHOULD_SKIP_THIS) || !defined(SL_ZIGBEE_SCRIPTED_TEST)
#endif // SILABS_EMBER_DEBUG_H
Macros#
This function is obsolete and no longer required to initialize the debug system.
Functions#
Print the filename and line number to the debug serial port.
Print the contents of RAM to the debug serial port.
Print binary data to the debug channel.
Send VUART data out the debug channel.
Print an ::sl_status_t return code to the serial port.
Turn off all debug output.
Restore the state of the debug output.
Prints text debug messages.
Function Documentation#
sl_zigbee_debug_assert#
void sl_zigbee_debug_assert (const char * filename, int linenumber)
Print the filename and line number to the debug serial port.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| const char * | N/A | filename | The name of the file where the assert occurred. |
| int | N/A | linenumber | The line number in the file where the assert occurred. |
sl_zigbee_debug_memory_dump#
void sl_zigbee_debug_memory_dump (uint8_t * start, uint8_t * end)
Print the contents of RAM to the debug serial port.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint8_t * | N/A | start | The start address of the block of RAM to dump. |
| uint8_t * | N/A | end | The end address of the block of RAM to dump (address of the last byte). |
sl_zigbee_debug_binary_printf#
void sl_zigbee_debug_binary_printf (const char * formatString, ... )
Print binary data to the debug channel.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| const char * | N/A | formatString | A string of conversion specification characters describing the arguments to be printed. |
| ... | N/A | The arguments to be printed. |
This function does not use the normal printf format conventions. To print text debug messages, use sl_zigbee_debug_printf(). The format string must contain only these conversion specification characters:
B - uint8_t value.
W - uint16_t value, printed least significant byte first.
D - uint32_t value, printed least significant byte first.
F - pointer to null terminated string in Flash (const char *).
xxxp - pointer to RAM, length is xxx (max 255).
lp - pointer to RAM, length is uint8_t argument.
xxxf - pointer to Flash (const char *), length is xxx (max 255).
lf - pointer to Flash (const char *), length is uint8_t argument.
b - sli_buffer_manager_buffer_t.
Examples:
sl_zigbee_debug_binary_printf("BWD", status, panId, channelMask);
sl_zigbee_debug_binary_printf("F8p", "string example", eui64);
sl_zigbee_debug_binary_printf("lp64fb", length, bytes, dataTable, buffer);
sli_util_debug_send_vuart_message#
void sli_util_debug_send_vuart_message (uint8_t * buff, uint8_t len)
Send VUART data out the debug channel.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint8_t * | N/A | buff | A pointer to the data to send. |
| uint8_t | N/A | len | The length of the data to send. |
sl_zigbee_debug_error#
void sl_zigbee_debug_error (sl_status_t code)
Print an ::sl_status_t return code to the serial port.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sl_status_t | N/A | code | The ::sl_status_t code to print. |
sl_zigbee_debug_report_off#
bool sl_zigbee_debug_report_off (void )
Turn off all debug output.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | N/A |
Returns
The current state (true for on, false for off).
sl_zigbee_debug_report_restore#
void sl_zigbee_debug_report_restore (bool state)
Restore the state of the debug output.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| bool | N/A | state | The state returned from sl_zigbee_debug_report_off(). This is done so that debug output is not blindly turned on. |
sl_zigbee_debug_printf#
void sl_zigbee_debug_printf (const char * formatString, ... )
Prints text debug messages.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| const char * | N/A | formatString | Takes the following: |
| ... | N/A |
%% | Percent sign |
|---|---|
%c | Single-byte char |
%s | RAM string |
%s | Flash string (does not follow the printf standard) |
%u | Two-byte unsigned decimal |
%d | Two-byte signed decimal |
%%02X, %%04X, %%08X | 1-, 2-, 4-byte hex value (always 0 padded; does not follow the printf standard) |