Lookup item structure for GPIO configuration.
This structure defines the lookup item for GPIO configuration, including port, pin, pin configuration, mode, interrupt settings, and callback information.
Public Attributes#
sl_gpio_t
int32_t
struct GPIO_PinConfig
sl_gpio_mode_t
bool
bool
struct GPIO_LookupItem::@1
void *
Public Attribute Documentation#
IntNO#
int32_t GPIO_LookupItem::IntNO
Interrupt number assigned by sl_gpio_configure_external_interrupt
PinConfig#
struct GPIO_PinConfig GPIO_LookupItem::PinConfig
Configuration parameters for the GPIO pin.
callback#
sid_pal_gpio_irq_handler_t GPIO_LookupItem::callback
Callback function to be called on GPIO interrupt.