Type definitions#
Modules#
Enumerations#
Values available to all users of the manufacturing store.
Value sizes in bytes.
Typedefs#
Function pointer type for converting an application-specific value to an offset.
Function pointer type for overwriting the default read calls.
Macros#
The current version of the MFG storage.
Last version with fixed offsets
This macro defines the version number for the TLV (Type-Length-Value)
Maximum length for flash write operations in the manufacturing store.
Enumeration Documentation#
sid_pal_mfg_store_value_t#
sid_pal_mfg_store_value_t
Values available to all users of the manufacturing store.
Enumerator | |
---|---|
SID_PAL_MFG_STORE_DEVID | use sid_pal_mfg_store_dev_id_get |
SID_PAL_MFG_STORE_VERSION | Note
|
SID_PAL_MFG_STORE_SERIAL_NUM | use sid_pal_mfg_store_dev_id_get |
SID_PAL_MFG_STORE_SMSN | |
SID_PAL_MFG_STORE_APP_PUB_ED25519 | |
SID_PAL_MFG_STORE_DEVICE_PRIV_ED25519 | |
SID_PAL_MFG_STORE_DEVICE_PUB_ED25519 | |
SID_PAL_MFG_STORE_DEVICE_PUB_ED25519_SIGNATURE | |
SID_PAL_MFG_STORE_DEVICE_PRIV_P256R1 | |
SID_PAL_MFG_STORE_DEVICE_PUB_P256R1 | |
SID_PAL_MFG_STORE_DEVICE_PUB_P256R1_SIGNATURE | |
SID_PAL_MFG_STORE_DAK_PUB_ED25519 | |
SID_PAL_MFG_STORE_DAK_PUB_ED25519_SIGNATURE | |
SID_PAL_MFG_STORE_DAK_ED25519_SERIAL | |
SID_PAL_MFG_STORE_DAK_PUB_P256R1 | |
SID_PAL_MFG_STORE_DAK_PUB_P256R1_SIGNATURE | |
SID_PAL_MFG_STORE_DAK_P256R1_SERIAL | |
SID_PAL_MFG_STORE_PRODUCT_PUB_ED25519 | |
SID_PAL_MFG_STORE_PRODUCT_PUB_ED25519_SIGNATURE | |
SID_PAL_MFG_STORE_PRODUCT_ED25519_SERIAL | |
SID_PAL_MFG_STORE_PRODUCT_PUB_P256R1 | |
SID_PAL_MFG_STORE_PRODUCT_PUB_P256R1_SIGNATURE | |
SID_PAL_MFG_STORE_PRODUCT_P256R1_SERIAL | |
SID_PAL_MFG_STORE_MAN_PUB_ED25519 | |
SID_PAL_MFG_STORE_MAN_PUB_ED25519_SIGNATURE | |
SID_PAL_MFG_STORE_MAN_ED25519_SERIAL | |
SID_PAL_MFG_STORE_MAN_PUB_P256R1 | |
SID_PAL_MFG_STORE_MAN_PUB_P256R1_SIGNATURE | |
SID_PAL_MFG_STORE_MAN_P256R1_SERIAL | |
SID_PAL_MFG_STORE_SW_PUB_ED25519 | |
SID_PAL_MFG_STORE_SW_PUB_ED25519_SIGNATURE | |
SID_PAL_MFG_STORE_SW_ED25519_SERIAL | |
SID_PAL_MFG_STORE_SW_PUB_P256R1 | |
SID_PAL_MFG_STORE_SW_PUB_P256R1_SIGNATURE | |
SID_PAL_MFG_STORE_SW_P256R1_SERIAL | |
SID_PAL_MFG_STORE_AMZN_PUB_ED25519 | |
SID_PAL_MFG_STORE_AMZN_PUB_P256R1 | |
SID_PAL_MFG_STORE_APID | |
SID_PAL_MFG_STORE_DTID | |
SID_PAL_MFG_STORE_CORE_VALUE_MAX | Note
|
SID_PAL_MFG_STORE_VALUE_MAX | Note
|
sid_pal_mfg_store_value_size_t#
sid_pal_mfg_store_value_size_t
Value sizes in bytes.
This enum defines the sizes of various values stored in the manufacturing store.
Enumerator | |
---|---|
SID_PAL_MFG_STORE_DEVID_SIZE | |
SID_PAL_MFG_STORE_VERSION_SIZE | |
SID_PAL_MFG_STORE_SERIAL_NUM_SIZE | |
SID_PAL_MFG_STORE_SMSN_SIZE | |
SID_PAL_MFG_STORE_APP_PUB_ED25519_SIZE | |
SID_PAL_MFG_STORE_DEVICE_PRIV_ED25519_SIZE | |
SID_PAL_MFG_STORE_DEVICE_PUB_ED25519_SIZE | |
SID_PAL_MFG_STORE_DEVICE_PUB_ED25519_SIGNATURE_SIZE | |
SID_PAL_MFG_STORE_DEVICE_PRIV_P256R1_SIZE | |
SID_PAL_MFG_STORE_DEVICE_PUB_P256R1_SIZE | |
SID_PAL_MFG_STORE_DEVICE_PUB_P256R1_SIGNATURE_SIZE | |
SID_PAL_MFG_STORE_DAK_PUB_ED25519_SIZE | |
SID_PAL_MFG_STORE_DAK_PUB_ED25519_SIGNATURE_SIZE | |
SID_PAL_MFG_STORE_DAK_ED25519_SERIAL_SIZE | |
SID_PAL_MFG_STORE_DAK_PUB_P256R1_SIZE | |
SID_PAL_MFG_STORE_DAK_PUB_P256R1_SIGNATURE_SIZE | |
SID_PAL_MFG_STORE_DAK_P256R1_SERIAL_SIZE | |
SID_PAL_MFG_STORE_PRODUCT_PUB_ED25519_SIZE | |
SID_PAL_MFG_STORE_PRODUCT_PUB_ED25519_SIGNATURE_SIZE | |
SID_PAL_MFG_STORE_PRODUCT_ED25519_SERIAL_SIZE | |
SID_PAL_MFG_STORE_PRODUCT_PUB_P256R1_SIZE | |
SID_PAL_MFG_STORE_PRODUCT_PUB_P256R1_SIGNATURE_SIZE | |
SID_PAL_MFG_STORE_PRODUCT_P256R1_SERIAL_SIZE | |
SID_PAL_MFG_STORE_MAN_PUB_ED25519_SIZE | |
SID_PAL_MFG_STORE_MAN_PUB_ED25519_SIGNATURE_SIZE | |
SID_PAL_MFG_STORE_MAN_ED25519_SERIAL_SIZE | |
SID_PAL_MFG_STORE_MAN_PUB_P256R1_SIZE | |
SID_PAL_MFG_STORE_MAN_PUB_P256R1_SIGNATURE_SIZE | |
SID_PAL_MFG_STORE_MAN_P256R1_SERIAL_SIZE | |
SID_PAL_MFG_STORE_SW_PUB_ED25519_SIZE | |
SID_PAL_MFG_STORE_SW_PUB_ED25519_SIGNATURE_SIZE | |
SID_PAL_MFG_STORE_SW_ED25519_SERIAL_SIZE | |
SID_PAL_MFG_STORE_SW_PUB_P256R1_SIZE | |
SID_PAL_MFG_STORE_SW_PUB_P256R1_SIGNATURE_SIZE | |
SID_PAL_MFG_STORE_SW_P256R1_SERIAL_SIZE | |
SID_PAL_MFG_STORE_AMZN_PUB_ED25519_SIZE | |
SID_PAL_MFG_STORE_AMZN_PUB_P256R1_SIZE | |
SID_PAL_MFG_STORE_APID_SIZE | |
SID_PAL_MFG_STORE_DTID_SIZE |
Typedef Documentation#
sid_pal_mfg_store_app_value_to_offset_t#
sid_pal_mfg_store_app_value_to_offset_t )(int value)
Function pointer type for converting an application-specific value to an offset.
Type | Direction | Argument Name | Description |
---|---|---|---|
N/A | value | The application-specific value to be converted to an offset. |
Returns
A 32-bit unsigned integer representing the offset corresponding to the input value.
sid_pal_mfg_store_overwrite_read_t#
sid_pal_mfg_store_overwrite_read_t )(uint16_t value, uint8_t *buffer, uint16_t length)
Function pointer type for overwriting the default read calls.
Type | Direction | Argument Name | Description |
---|---|---|---|
N/A | value | Enum constant for the desired value. Use values from sid_pal_mfg_store_value_t or application defined values here. | |
N/A | buffer | Buffer to which the value will be copied. | |
N/A | length | Length of the value in bytes. Use values from sid_pal_mfg_store_value_size_t here. |
Returns
True if the value is overwritten, otherwise false