You are viewing documentation for version:
PDFParameters for ECC DSA cryptographic operations.
This structure defines the parameters required for ECC DSA cryptographic operations supported by the SID PAL (Platform Abstraction Layer).
Public Attribute Documentation#
algo#
sid_pal_ecc_algo_t sid_pal_dsa_params_t::algo
ECC algorithm to be used
mode#
sid_pal_dsa_mode_t sid_pal_dsa_params_t::mode
DSA mode of operation
key#
uint8_t const* sid_pal_dsa_params_t::key
Pointer to the key
key_size#
size_t sid_pal_dsa_params_t::key_size
Size of the key
uint8_t const* sid_pal_dsa_params_t::in
Pointer to the input data
in_size#
size_t sid_pal_dsa_params_t::in_size
Size of the input data
signature#
uint8_t* sid_pal_dsa_params_t::signature
Pointer to the signature
sig_size#
size_t sid_pal_dsa_params_t::sig_size
Size of the signature