You are viewing documentation for version:
PDFSidewalk Phy transmit packet configuration.
Public Attribute Documentation#
packet_cfg#
sid_pal_radio_packet_cfg_t sid_pal_radio_tx_packet_t::packet_cfg
Configuration for the packet
tx_power_in_dbm#
int8_t sid_pal_radio_tx_packet_t::tx_power_in_dbm
Transmit power in dBm
tx_payload#
uint8_t* sid_pal_radio_tx_packet_t::tx_payload
Pointer to the payload to be transmitted
payload_len#
uint8_t sid_pal_radio_tx_packet_t::payload_len
Length of the payload
timeout#
uint32_t sid_pal_radio_tx_packet_t::timeout
Timeout for the transmission