Prerequisites#

To develop for Amazon Sidewalk on Silicon Labs SoCs and modules, you need the hardware and software resources detailed on this page.

Hardware#

Silicon Labs Wireless Development Hardware#

Silicon Labs produces many different kits to support development for a broad range of wireless technologies. New users can jump-start their journey with a Silicon Labs Pro Kit for Amazon Sidewalk. While experienced users may have much of the required hardware on hand already, Silicon Labs recommends they too start with Silicon Labs Pro Kit for Amazon Sidewalk.

For Amazon Sidewalk solutions, the typical Silicon Labs development hardware is a wireless main board paired with a radio board that supports Sidewalk. The Sidewalk-specific wireless technologies supported in this configuration (Bluetooth Low Energy (BLE), sub-GHz FSK, and sub-GHz CSS) depend on the radio board, as shown in the following table. Note that for sub-GHz support, some devices will require both an EFR32 radio board and an additional Semtech LoRa shield with the appropriate adapter board. Advanced users who have already bought a Pro Kit or have a WSTK/WPK can augment their existing hardware with additional radio boards as needed.

The following list and table summarizes these requirements. You can also read our hardware selector guide to help choose appropriate hardware for your use case.

Radio Board Family

BLE

RAIL FSK

SX1262 (FSK + CSS)

LR1110 (FSK + CSS)

EFR32xG21 Series

*

*

EFR32xG23 Series

*

*

EFR32xG24 Series

*

*

EFR32xG25 Series

EFR32xG26 Series

*

*

EFR32xG27 Series

EFR32xG28 Series

*

*

EFR32xG29 Series

KG100S (Quectel)

Ⓘ INFO Ⓘ: BLE and RAIL FSK are supported natively on selected Silicon Labs SoCs. Support for CSS requires external hardware such as SX1262 and LR1110.

⚠ WARNING ⚠: Only one Sub-GHz radio solution can be active at a time —RAIL FSK, SX1262, or LR1110. However, BLE can operate concurrently with any of the Sub-GHz options.

Ⓘ INFO Ⓘ: Amazon Sidewalk support requires that target hardware have Secure Element (SE) firmware versions of at least v1.2.9 for xG21 SoCs, v2.1.7 for xG24 SoCs, and v1.2.9 for KG100S Modules. Follow instructions in Section 4.4 of AN1222: Production Programming of Series 2 Devices to update the SE firmware. xG28 and xG23 should come with an appropriate SE firmware version.

⚠ WARNING ⚠: Several family are available with various flash sizes. Minimum flash size to run the Hello Neighbor example applications is 768 kB. This restriction does not apply to EFR32xG23 devices, which do not support BLE.

For simplicity, this Getting Started Guide focuses on the EFR32MG24 and demonstrates how to use the Amazon Sidewalk - SoC Hello Neighbor example application provided in the SDK for Amazon Sidewalk.

Amazon Sidewalk Gateway#

The Sidewalk protocol requires a gateway to provide endpoints access to the AWS cloud. Several Amazon products can act as a gateway. These products have different functions and varying support for Amazon Sidewalk network features. The list of Amazon Sidewalk gateways and their supported radio capabilities is available at the following link: https://docs.sidewalk.amazon/introduction/sidewalk-gateways.html.

The Ring Bridge 2nd generation is the recommended Amazon Sidewalk gateway for development purposes.

Developers are advised to use their own gateway, as this affords the greatest control over providing consistent network access during the development phase. However, you may already have access to the Amazon Sidewalk network at your location. Amazon provides a Sidewalk Network Coverage map you can use to see if this is likely: https://coverage.sidewalk.amazon.

Sidewalk Gateway Setup#

Follow the standard product installation procedures to set up a new gateway. Configuring your gateway with Sidewalk support depends on a few additional requirements:

Using Sidewalk Gateways Outside the USA#

⚠ WARNING ⚠: Amazon Sidewalk is available only in the United States of America. To the extent that any Sidewalk gateway functionality might be used outside of the U.S., it should be used ONLY for Amazon Sidewalk endpoint development purposes. In addition, Silicon Labs recommends that you consult with your local regulatory bodies and check if the gateway is allowed to operate its radio in your locale, as U.S. license-free band devices, only for development. Developers are solely responsible for ensuring compliance with local regulations. Additionally, Silicon Labs recommends a shielded chamber or similar aparatus to capture and contain wireless signals within your development environment.

To enable operation outside of the US for your development, you need to use a VPN router that supports OpenVPN Client functionality in conjunction with a cloud VPN service provider. Refer to the following Amazon documentation for more details. You are also solely responsible for compliance with any local regulations regarding VPN use.

Ⓘ INFO Ⓘ: VPN clients running on a laptop or mobile device or using any other VPN protocol (such as L2TP or PPTP) are not supported.

Amazon Frustration-Free Setup (FFS)#

A fully operational gateway is linked to an Amazon account, usually during initial setup using the Alexa app. However, this device-account linking can instead be initiated at time of purchase if you buy the gateway from Amazon and check the box labeled Link device to your Amazon account to simplify setup. This account linking has implications for Sidewalk feature support and gateway setup:

  • Currently, FSK support is enabled on only one (by default, the first) compatible gateway linked to an account.

  • If you purchase a gateway device using an Amazon account other than the one you plan to use for testing and in the Alexa app to configure the gateway, do NOT check the Link device to your Amazon account box. Doing so may prevent the successful setup of your gateway until you request Amazon Customer Support to remove the original device-account link. More info: Amazon Frustration-Free Setup Frequently Asked Questions.

  • The Link device checkbox also enables Amazon Wi-Fi Simple Setup, which can simplify getting your new gateway connected when powered on. However, if you plan to connect the gateway to a different SSID than you already use with other devices known to your Amazon account, the FFS-driven automatic selection of Wi-Fi networks can impede your efforts to connect the gateway to your preferred SSID.

Software#

To get started with your Amazon Sidewalk development, you need:

Ⓘ INFO Ⓘ: Amazon Sidewalk support requires the Amazon Sidewalk SDK extension. The extension version 1.0.0 requires at least Simplicity Studio 5, the Simplicity Commander version included in that release, GSDK 4.2.2, and JLink version 7.84. However, starting with Simplicity SDK 2025.12, only Studio 6 is supported.

Silicon Labs SDK Extension for Amazon Sidewalk#

During the initial install of Simplicity Studio, with the new package manager concept, support for Amazon Sidewalk can be added with Simplicity Installer by either selecting PACKAGE MANAGER or INSTALLATION WIZARD.

Simplicity InstallerSimplicity Installer

The following presents the fastest way to have the SDK extension for Amazon Sidewalk up and running.

If Simplicity Studio 6 is not installed yet#

  1. Open Simplicity Installer.

  2. Select INSTALLATION WIZARD.

    Installation WizardInstallation Wizard

  3. Select TECHNOLOGY INSTALL.

    Installation WizardInstallation Wizard

  4. Select Sidewalk from the OPTIONAL PACKAGES, click NEXT.

    Technology InstallTechnology Install

  5. Select the checkbox for the Terms Of Service and License Agreement and click INSTALL.

    Technology Install 2Technology Install 2

  6. Wait for the installation to complete. When the installation is completed, "Successful Installation!" message displays.

  7. Verify the installed Simplicity SDK and Sidewalk support under the installed SDK packages.

  8. Click CLOSE or LAUNCH STUDIO.

    Technology Install 3Technology Install 3

If Simplicity Studio 6 is already installed#

  1. Open Simplicity Studio 6.

  2. If Simplicity Studio 6 was installed by TECHNOLOGY INSTALL or FULL INSTALL, Simplicity SDK is also already installed.

  3. Verify the installed Simplicity SDK is the latest, by clicking on SETTINGS, then select SDKs.

    Studio PackagesStudio Packages

If a different Simplicity SDK version is installed or no Simplicity SDK is installed, click PACKAGES:

  1. Simplicity Installer opens, click PACKAGE MANAGER.

  2. Under SDK select Simplicity SDKs, then click on Add new SDK.

  3. Select the latest version from the Versions list.

  4. Check the Simplicity SDK... from the list.

  5. Here the latest Sidewalk SDK extension Sidewalk... also can be selected / checked in the list in the same step.

  6. Click INSTALL.

    Simplicity SDKSimplicity SDK

  7. Wait for the installation to complete.

Otherwise, repeat the previous steps, without the need for: "Check the Simplicity SDK... from the list", since it will be shown as already installed.

Simplicity SDKSimplicity SDK

Do not forget to install Visual Studio Code and Visual Studio Code extension, the primary companion tool for application development for Simplicity Studio 6.

AWS Command Line Interface (CLI)#

To perform the operations that create and manage the cloud-based elements of your Amazon Sidewalk applications, your scripts and the Sidewalk Assistant use AWS CLI. With the AWS CLI, these tools can run commands that implement functionality equivalent to that provided by the browser-based AWS Management Console. Use the resources below to set up AWS CLI for these purposes.

Ⓘ INFO Ⓘ: Note that Amazon has currently activated Sidewalk only for the North Virginia region ("us-east-1"). To support Sidewalk development (and operation), your AWS CLI and AWS web interface should be localized on this us-east-1 region.

  • Prerequisites to use the AWS CLI. To prepare your system to support AWS CLI, you must create users in your AWS CLI account. For convenience, Silicon Labs recommends using long-term IAM credentials (via IAM) to access AWS during your evaluation:

    1. Follow the guidance in Getting set up with IAM to create an AWS account if you do not already have one.

    2. Follow steps 1 thru 3 in Authenticate using long-term credentials to create an administrator IAM account (select the AdministratorAccess policy), get your access keys, and update the shared credentials file. (For additional assistance on these topics, see Getting started with IAM and Managing access keys for IAM users)

  • Install AWS CLI. If AWS CLI is not already installed, install it as described here.

  • Configure AWS CLI. Configure AWS CLI to leverage your IAM administrator account. (Sidewalk Assistant supports the recommended credentials file approach described in prior bullets and environment variables (except on Mac OS where environment variables are not supported).)

Getting Support#

Silicon Labs supports developers in many ways, including with documentation and active community forums where other users and Silicon Labs employees offer guidance to those in need.

Taking the Next Step#

Once you have completed the required hardware and software setup tasks, you can begin creating and compiling an Amazon Sidewalk Application.