Uptime#
The Uptime Interface module provides interfaces for tracking and managing system uptime within the Sidewalk SDK. These interfaces ensure consistent and platform-independent access to uptime information, allowing developers to monitor the duration for which the system has been running since the last reset or power cycle.
Functions#
sid_error_t
sid_pal_uptime_now(struct sid_timespec *time)
Get the current time of specified clock source.
void
sid_pal_uptime_set_xtal_ppm(int16_t ppm)
Set crystal offset for RTC compensation.
int16_t
Get current crystal offset.
Function Documentation#
sid_pal_uptime_now#
sid_error_t sid_pal_uptime_now (struct sid_timespec * time)
Get the current time of specified clock source.
Parameters
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| struct sid_timespec * | [out] | time | current time |
NOTE: drift may be NULL. In this case time should be set and drift ignored. Success should be returned.
sid_pal_uptime_set_xtal_ppm#
void sid_pal_uptime_set_xtal_ppm (int16_t ppm)
Set crystal offset for RTC compensation.
Parameters
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| int16_t | [in] | ppm | offset in PPM |
sid_pal_uptime_get_xtal_ppm#
int16_t sid_pal_uptime_get_xtal_ppm (void )
Get current crystal offset.
Parameters
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | N/A |