Repositories#
The hardware drivers and application examples are stored on Github in public Git repositories.
Hardware Drivers#
These are drivers for third-party devices such as sensors, displays, and interfaces for various types of hardware.
Deprecated repository, the newly developed drivers for the application examples are stored in the Third-Party Hardware Drivers GSDK Extension.
https://github.com/SiliconLabs/platform_hardware_drivers
Third-Party Hardware Drivers - GSDK Extension#
SDK Extension for Third-Party hardware drivers for EFM32 and EFR32.
https://github.com/SiliconLabs/third_party_hw_drivers_extension
Wireless Applications by technology#
The Application Examples Program provides real-life application examples for most of the popular wireless technologies. These examples are stored in separate repositories.
https://github.com/SiliconLabs/application_examples
Bluetooth#
Proprietary#
Thread#
Wi-Fi#
Zigbee#
Z-Wave#
Matter#
EFM32-EFR32 Platform#
Utilities and Training Materials#
Trainings
IoT Utilities