Data structure of the boot event.

Public Attributes#

uint16_t
uint16_t
uint16_t
uint16_t
uint32_t
uint16_t
uint32_t

Public Attribute Documentation#

major#

uint16_t sl_bt_evt_system_boot_s::major

Major release version


minor#

uint16_t sl_bt_evt_system_boot_s::minor

Minor release version


patch#

uint16_t sl_bt_evt_system_boot_s::patch

Patch release number


build#

uint16_t sl_bt_evt_system_boot_s::build

This parameter is unused. Set to 0 always.


bootloader#

uint32_t sl_bt_evt_system_boot_s::bootloader

Bootloader version if a bootloader is present in the application. Set to 0 if bootloader is not present.


hw#

uint16_t sl_bt_evt_system_boot_s::hw

Hardware type: the major chip revision number in the most significant byte and the minor revision in the least significant byte


hash#

uint32_t sl_bt_evt_system_boot_s::hash

Version hash