GATT Send Options#
Defines the option flags used with sl_bt_gatt_server_send_notification_with_options and sl_bt_gatt_server_send_indication_with_options.
Macros#
#define
Perform the standard notification or indication procedure.
#define
Send the notification or indication regardless of whether the corresponding configuration in the Client Characteristic Configuration of the connected client has been set.
Macro Definition Documentation#
SL_BT_GATT_SERVER_SEND_OPTION_NONE#
#define SL_BT_GATT_SERVER_SEND_OPTION_NONEValue:
0x0
Perform the standard notification or indication procedure.
SL_BT_GATT_SERVER_SEND_OPTION_IGNORE_CCCD#
#define SL_BT_GATT_SERVER_SEND_OPTION_IGNORE_CCCDValue:
0x1
Send the notification or indication regardless of whether the corresponding configuration in the Client Characteristic Configuration of the connected client has been set.