Data structure of the opened event.
Public Attribute Documentation#
address_type#
uint8_t sl_bt_evt_periodic_sync_opened_s::address_type
Enum sl_bt_gap_address_type_t.
Advertiser address type.
If the application does not include the bluetooth_feature_use_accurate_api_address_types component, address_type uses the following values:
- 0: Public address 
- 1: Random address 
If the application includes the bluetooth_feature_use_accurate_api_address_types component, address_type uses enum sl_bt_gap_address_type_t values:
- sl_bt_gap_public_address (0x0): Public device address 
- sl_bt_gap_static_address (0x1): Static device address 
- sl_bt_gap_random_resolvable_address (0x2): Resolvable private random address 
- sl_bt_gap_random_nonresolvable_address (0x3): Non-resolvable private random address 
- sl_bt_gap_public_address_resolved_from_rpa (0x4): Public identity address resolved from a resolvable private address (RPA) 
- sl_bt_gap_static_address_resolved_from_rpa (0x5): Static identity address resolved from a resolvable private address (RPA) 
adv_phy#
uint8_t sl_bt_evt_periodic_sync_opened_s::adv_phy
Enum sl_bt_gap_phy_t. The advertiser PHY. Values:
- sl_bt_gap_phy_1m (0x1): 1M PHY 
- sl_bt_gap_phy_2m (0x2): 2M PHY 
- sl_bt_gap_phy_coded (0x4): Coded PHY, 125k (S=8) or 500k (S=2) 
adv_interval#
uint16_t sl_bt_evt_periodic_sync_opened_s::adv_interval
The Periodic Advertising interval. Value in units of 1.25 ms
- Range: 0x06 to 0xFFFF 
- Time range: 7.5 ms to 81.92 s 
clock_accuracy#
uint16_t sl_bt_evt_periodic_sync_opened_s::clock_accuracy
Enum sl_bt_sync_advertiser_clock_accuracy_t. The advertiser clock accuracy.
bonding#
uint8_t sl_bt_evt_periodic_sync_opened_s::bonding
Bonding handle. Values:
- SL_BT_INVALID_BONDING_HANDLE (0xff): No bonding 
- Other: Bonding handle