CS ACP#

Channel Sounding (CS) Application Co-Processor (ACP) provides the ACP commands and events to the CS device roles.

Modules#

cs_acp_get_target_config_rsp_t

cs_acp_cmd_t

cs_acp_result_evt_t

cs_acp_intermediate_result_evt_t

cs_acp_extended_result_evt_t

cs_acp_status_t

cs_acp_event_t

CS ACP commands#

Command enumerator defines the available ACP commands between the host application and target device.

enum
CS_ACP_CMD_CREATE_INITIATOR = 0
CS_ACP_CMD_CREATE_REFLECTOR = 1
CS_ACP_CMD_INITIATOR_ACTION = 2
CS_ACP_CMD_REFLECTOR_ACTION = 3
CS_ACP_CMD_ANTENNA_CONFIGURE = 4
CS_ACP_CMD_ENABLE_TRACE = 5
CS_ACP_CMD_GET_TARGET_CONFIG = 6
}

ACP initiator actions#

Initiator role related action enumerator.

enum
CS_ACP_ACTION_DELETE_INITIATOR = 0
}

ACP reflector actions#

Reflector role related action enumerator.

enum
CS_ACP_ACTION_DELETE_REFLECTOR = 0
}

CS ACP event enumerator#

Event enumerator defines the available ACP events coming from target device to the host application.

enum
CS_ACP_EVT_RESULT_ID = 0
CS_ACP_EVT_STATUS_ID = 1
CS_ACP_EVT_INTERMEDIATE_RESULT_ID = 2
CS_ACP_EVT_EXTENDED_RESULT_ID = 3
}

Variables#

uint8_t

Target config bitfield.

uint8_t

Maximum initiator instance count.

uint8_t

Maximum BLE connections.

CS ACP command enumerator.

uint8_t

Antenna configuration for wired offset.

uint8_t

Antenna configuration for wired offset.

uint8_t

Enable BGAPI trace feature.

uint8_t

Enable BGAPI trace feature.

union cs_acp_cmd_t::@1
uint8_t

Result data in type-value pairs.

float

Progress percentage.

uint8_t

Number of fragments left.

uint8array

Content of the fragment.

uint32_t

Status code.

uint8_t

Error code.

uint8_t

Connection ID.

CS ACP event enumerator.

Result event data.

Result event data.

Extended result event data.

Extended result event data.

Status change event data.

Status change event data.

union cs_acp_event_t::@2

Macros#

#define

The MSB of the fragments_left field indicates the start of a fragmented message.

#define

The remaining bits of the fragments_left field indicate the number of fragments left.

#define

Bitmask for the RAS mode bit in the target config.

CS ACP commands Documentation#

cs_acp_cmd_id_t#

cs_acp_cmd_id_t
Enumerator
CS_ACP_CMD_CREATE_INITIATOR

Create initiator instance.

CS_ACP_CMD_CREATE_REFLECTOR

Create reflector instance.

CS_ACP_CMD_INITIATOR_ACTION

Initiator action (eg. delete instance)

CS_ACP_CMD_REFLECTOR_ACTION

Reflector action (eg. delete instance)

CS_ACP_CMD_ANTENNA_CONFIGURE

Configure antenna.

CS_ACP_CMD_ENABLE_TRACE

Enable BGAPI trace feature.

CS_ACP_CMD_GET_TARGET_CONFIG

Get ACP target configuration.


ACP initiator actions Documentation#

cs_acp_initiator_action_t#

cs_acp_initiator_action_t
Enumerator
CS_ACP_ACTION_DELETE_INITIATOR

Delete initiator instance.


ACP reflector actions Documentation#

cs_acp_reflector_action_t#

cs_acp_reflector_action_t
Enumerator
CS_ACP_ACTION_DELETE_REFLECTOR

Delete reflector instance.


CS ACP event enumerator Documentation#

cs_acp_event_id_t#

cs_acp_event_id_t
Enumerator
CS_ACP_EVT_RESULT_ID

Result event (includes distance, likeliness etc.)

CS_ACP_EVT_STATUS_ID

Status change event (error, success etc.)

CS_ACP_EVT_INTERMEDIATE_RESULT_ID

Intermediate result event (progress percentage)

CS_ACP_EVT_EXTENDED_RESULT_ID

Extended result event (fragments)


Variable Documentation#

target_config_bitfield#

uint8_t cs_acp_get_target_config_rsp_t::target_config_bitfield

Target config bitfield.


max_initiator_instance_count#

uint8_t cs_acp_get_target_config_rsp_t::max_initiator_instance_count

Maximum initiator instance count.


max_bluetooth_connections#

uint8_t cs_acp_get_target_config_rsp_t::max_bluetooth_connections

Maximum BLE connections.


cmd_id#

cs_acp_cmd_id_t cs_acp_cmd_t::cmd_id

CS ACP command enumerator.


antenna_config_wired#

uint8_t cs_acp_cmd_t::antenna_config_wired

Antenna configuration for wired offset.


antenna_config_wired#

uint8_t cs_acp_cmd_t::@1::antenna_config_wired

Antenna configuration for wired offset.


enable_trace#

uint8_t cs_acp_cmd_t::enable_trace

Enable BGAPI trace feature.


enable_trace#

uint8_t cs_acp_cmd_t::@1::enable_trace

Enable BGAPI trace feature.


data#

union cs_acp_cmd_t::@1 cs_acp_cmd_t::data

type_value_list#

uint8_t cs_acp_result_evt_t::type_value_list[CS_RESULT_MAX_BUFFER_SIZE]

Result data in type-value pairs.


progress_percentage#

float cs_acp_intermediate_result_evt_t::progress_percentage

Progress percentage.


fragments_left#

uint8_t cs_acp_extended_result_evt_t::fragments_left

Number of fragments left.


fragment#

uint8array cs_acp_extended_result_evt_t::fragment

Content of the fragment.


sc#

uint32_t cs_acp_status_t::sc

Status code.


error#

uint8_t cs_acp_status_t::error

Error code.


connection_id#

uint8_t cs_acp_event_t::connection_id

Connection ID.


acp_evt_id#

cs_acp_event_id_t cs_acp_event_t::acp_evt_id

CS ACP event enumerator.


result#

cs_acp_result_evt_t cs_acp_event_t::result

Result event data.


result#

cs_acp_result_evt_t cs_acp_event_t::@2::result

Result event data.


intermediate_result#

cs_acp_intermediate_result_evt_t cs_acp_event_t::intermediate_result

Intermediate result event data.


intermediate_result#

cs_acp_intermediate_result_evt_t cs_acp_event_t::@2::intermediate_result

Intermediate result event data.


ext_result#

cs_acp_extended_result_evt_t cs_acp_event_t::ext_result

Extended result event data.


ext_result#

cs_acp_extended_result_evt_t cs_acp_event_t::@2::ext_result

Extended result event data.


stat#

cs_acp_status_t cs_acp_event_t::stat

Status change event data.


stat#

cs_acp_status_t cs_acp_event_t::@2::stat

Status change event data.


data#

union cs_acp_event_t::@2 cs_acp_event_t::data

Macro Definition Documentation#

CS_ACP_FIRST_FRAGMENT_MASK#

#define CS_ACP_FIRST_FRAGMENT_MASK
Value:
0x80

The MSB of the fragments_left field indicates the start of a fragmented message.


CS_ACP_FRAGMENTS_LEFT_MASK#

#define CS_ACP_FRAGMENTS_LEFT_MASK
Value:
0x7F

The remaining bits of the fragments_left field indicate the number of fragments left.


CS_ACP_TARGET_CONFIG_RAS_MODE_BIT_POS#

#define CS_ACP_TARGET_CONFIG_RAS_MODE_BIT_POS
Value:
0x00

Bitmask for the RAS mode bit in the target config.