CS Reflector#
Channel Sounding (CS) Reflector role implementation for all BLE Channel Sounding apps.
Modules#
Functions#
Macros#
Function Documentation#
cs_reflector_identify#
bool cs_reflector_identify (uint8_t conn_handle)
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint8_t | [in] | conn_handle | the connection handle to identify |
Determine whether a connection handle has a reflector associated to it
Returns
trueif the handle has an associated reflector instance,falseotherwise
cs_reflector_create#
sl_status_t cs_reflector_create (uint8_t conn_handle, cs_reflector_config_t * reflector_config)
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint8_t | [in] | conn_handle | the connection handle for which to create the reflector |
| cs_reflector_config_t * | [in] | reflector_config | reflector configuration parameters |
Create a reflector for the given connection handle
Returns
status of the operation
cs_reflector_get_active_instance_count#
uint8_t cs_reflector_get_active_instance_count (void )
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | N/A |
Get the number of active reflector instances
Returns
the number of active reflector instances
cs_reflector_delete#
sl_status_t cs_reflector_delete (uint8_t conn_handle)
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint8_t | [in] | conn_handle | the connection handle for which to delete the reflector |
Delete the reflector associated with the given connection handle
Returns
status of the operation
cs_reflector_on_bt_event#
bool cs_reflector_on_bt_event (sl_bt_msg_t * evt)
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sl_bt_msg_t * | [in] | evt | the Bluetooth stack event to handle |
Handle a Bluetooth stack event
Returns
true to forward the message to the host in NCP case
cs_rcm_get_connection_ctx#
connection_ctx_t * cs_rcm_get_connection_ctx (const uint8_t conn_handle)
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| const uint8_t | [in] | conn_handle | the connection handle to search for |
Find the pointer to a connection context which belongs to the provided connection handle.
Returns
the pointer of the context corresponding to the provided connection handle, NULL if not found
cs_rcm_add_new_initiator_connection#
sl_status_t cs_rcm_add_new_initiator_connection (const uint8_t conn_handle)
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| const uint8_t | [in] | conn_handle | the connection handle to register |
Register a new initiator connection with the provided handle.
Returns
status of the operation
cs_rcm_remove_initiator_connection#
void cs_rcm_remove_initiator_connection (const uint8_t conn_handle)
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| const uint8_t | [in] | conn_handle | the connection handle to remove |
Remove an initiator connection with the provided handle.
cs_rcm_can_accept_new_connection#
bool cs_rcm_can_accept_new_connection (void )
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | N/A |
Tell whether an additional connection can be accepted.
Returns
true if an additional connection can be accepted, false otherwise
cs_rcm_get_number_of_connections#
uint8_t cs_rcm_get_number_of_connections (void )
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | N/A |
Show the number of active connections.
Returns
the number of active connections