User Messaging#

User Messaging.

This class provides commands and events, which can be used by a NCP host and target to implement a communication mechanism with a custom proprietary protocol. An application must decide whether and how the command and event are used. The Bluetooth host stack does not produce or consume any messages belonging to this class.

Modules#

sl_bt_evt_user_message_to_host

sl_bt_evt_user_cs_service_message_to_host

Functions#

sl_status_t
sl_bt_user_message_to_target(size_t data_len, const uint8_t *data, size_t max_response_size, size_t *response_len, uint8_t *response)
sl_status_t
sl_bt_user_manage_event_filter(size_t data_len, const uint8_t *data)
sl_status_t
sl_bt_user_cs_service_message_to_target(size_t data_len, const uint8_t *data, size_t max_response_size, size_t *response_len, uint8_t *response)

Function Documentation#

sl_bt_user_message_to_target#

sl_status_t sl_bt_user_message_to_target (size_t data_len, const uint8_t * data, size_t max_response_size, size_t * response_len, uint8_t * response)
Parameters
TypeDirectionArgument NameDescription
size_t[in]data_len

Length of data in data

const uint8_t *[in]data

The message

size_t[in]max_response_size

Size of output buffer passed in response

size_t *[out]response_len

On return, set to the length of output data written to response

uint8_t *[out]response

The response message

Used by an NCP host to send a message to the target application on device. The application on the target must send the response with sl_bt_send_rsp_user_message_to_target.

Returns

  • SL_STATUS_OK if successful. Error code otherwise.


sl_bt_user_manage_event_filter#

sl_status_t sl_bt_user_manage_event_filter (size_t data_len, const uint8_t * data)
Parameters
TypeDirectionArgument NameDescription
size_t[in]data_len

Length of data in data

const uint8_t *[in]data

The message for managing event filter

Manage NCP event filter. When the event filter is in use, API events passing the filter will be sent to the host and those that do not pass are discarded by the target. For functionality details, see the NCP component in the Bluetooth SDK.

By default, the NCP does not use the event filter.

Returns

  • SL_STATUS_OK if successful. Error code otherwise.


sl_bt_user_reset_to_dfu#

void sl_bt_user_reset_to_dfu (void )
Parameters
TypeDirectionArgument NameDescription
voidN/A

Reset the target device to DFU mode from the NCP host. This command is used by specific SDK DFU component on the target device for the functionality related to DFU. Do not use it in other circumstances. This command does not have a response.


sl_bt_user_cs_service_message_to_target#

sl_status_t sl_bt_user_cs_service_message_to_target (size_t data_len, const uint8_t * data, size_t max_response_size, size_t * response_len, uint8_t * response)
Parameters
TypeDirectionArgument NameDescription
size_t[in]data_len

Length of data in data

const uint8_t *[in]data

The message

size_t[in]max_response_size

Size of output buffer passed in response

size_t *[out]response_len

On return, set to the length of output data written to response

uint8_t *[out]response

The response message

Used by an NCP host to send a message to the Channel Sounding service component on target device. The Channel Sounding service on target device must send the response with sl_bt_send_rsp_user_cs_service_message_to_target.

Returns

  • SL_STATUS_OK if successful. Error code otherwise.


Macro Definition Documentation#

sl_bt_cmd_user_message_to_target_id#

#define sl_bt_cmd_user_message_to_target_id
Value:
0x00ff0020

sl_bt_cmd_user_manage_event_filter_id#

#define sl_bt_cmd_user_manage_event_filter_id
Value:
0x01ff0020

sl_bt_cmd_user_reset_to_dfu_id#

#define sl_bt_cmd_user_reset_to_dfu_id
Value:
0x02ff0020

sl_bt_cmd_user_cs_service_message_to_target_id#

#define sl_bt_cmd_user_cs_service_message_to_target_id
Value:
0x03ff0020

sl_bt_rsp_user_message_to_target_id#

#define sl_bt_rsp_user_message_to_target_id
Value:
0x00ff0020

sl_bt_rsp_user_manage_event_filter_id#

#define sl_bt_rsp_user_manage_event_filter_id
Value:
0x01ff0020

sl_bt_rsp_user_reset_to_dfu_id#

#define sl_bt_rsp_user_reset_to_dfu_id
Value:
0x02ff0020

sl_bt_rsp_user_cs_service_message_to_target_id#

#define sl_bt_rsp_user_cs_service_message_to_target_id
Value:
0x03ff0020