Data structure of the report event.
Public Attribute Documentation#
analyzer#
uint8_t sl_bt_evt_connection_analyzer_report_s::analyzer
The handle of the connection analyzer
central_rssi#
int8_t sl_bt_evt_connection_analyzer_report_s::central_rssi
RSSI measurement of the packet transmitted by central in units dBm, or 127 if the packet was not observed.
Range: -127 to +20
Value 127: RSSI information unavailable
peripheral_rssi#
int8_t sl_bt_evt_connection_analyzer_report_s::peripheral_rssi
RSSI measurement of the packet transmitted by peripheral in units dBm, or 127 if the packet was not observed.
Range: -127 to +20
Value 127: RSSI information unavailable