CS Antenna#
Channel Sounding (CS) Antenna manages CS antenna offset settings.
Function Documentation#
cs_antenna_configure#
sl_status_t cs_antenna_configure (bool wired)
Parameters
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| bool | [in] | wired | Use wireless offset values if false, wired otherwise. |
Configure antenna offset values.
Can be called only after the Bluetooth system boot event has arrived.
cs_antenna_on_bt_event#
bool cs_antenna_on_bt_event (sl_bt_msg_t * evt)
Parameters
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sl_bt_msg_t * | [in] | evt | Bluetooth event. |
Bluetooth event handler of the CS Antenna component. Registered automatically via the bluetooth_on_event template contribution.
Returns
Always returns false; the event is left for further processing by other handlers.