Data structure of the subevent_report event.
Public Attribute Documentation#
tx_power#
int8_t sl_bt_evt_pawr_sync_subevent_report_s::tx_power
TX power value in the received packet header. Units: dBm
Range: -127 to 126
Value 127: information unavailable
rssi#
int8_t sl_bt_evt_pawr_sync_subevent_report_s::rssi
Signal strength indicator (RSSI) of the received packet. Units: dBm
Range: -127 to +20
cte_type#
uint8_t sl_bt_evt_pawr_sync_subevent_report_s::cte_type
The CTE type
0x00: AoA CTE
0x01: AoD CTE with 1us slots
0x02: AoD CTE with 2us slots
0xFF: No CTE
event_counter#
uint16_t sl_bt_evt_pawr_sync_subevent_report_s::event_counter
The value of the periodic advertising event counter (paEventCounter) of the event in which the advertisement was received. If the application responds to this advertisement, use this field as the value of request_event parameter for the sl_bt_pawr_sync_set_response_data command.
subevent#
uint8_t sl_bt_evt_pawr_sync_subevent_report_s::subevent
The subevent in which the advertisement was received. If the application responds to this advertisement, use this field as the value of request_subevent parameter for the sl_bt_pawr_sync_set_response_data command.
data_status#
uint8_t sl_bt_evt_pawr_sync_subevent_report_s::data_status
Enum sl_bt_pawr_sync_subevent_data_status_t. The subevent data completeness status. Values:
sl_bt_pawr_sync_subevent_data_status_complete (0x0): All data of the PAwR subevent has been reported.
sl_bt_pawr_sync_subevent_data_status_incomplete_more (0x1): Data of the PAwR subevent is incomplete in this event, and more data will come in new events.
sl_bt_pawr_sync_subevent_data_status_incomplete_nomore (0x2): Data of the PAwR subevent is incomplete in this event, but no more data will come, i.e., the data of the PAwR subevent is truncated.
sl_bt_pawr_sync_subevent_data_status_not_received (0xff): Failed to receive subevent data in this subevent.
counter#
uint8_t sl_bt_evt_pawr_sync_subevent_report_s::counter
The sequence number of this sl_bt_evt_pawr_sync_subevent_report event as a monotonically increasing counter that wraps from 255 to 0. There is a single counter for this event type that starts from value 0 when the Bluetooth stack is started and is never reset while the stack is running. This counter can be used to detect if one or more sl_bt_evt_pawr_sync_subevent_report events have been created by the stack but dropped due to problems such as temporarily running out of resources before the event reached the application.