BLE Peer Manager Central#
Peer Manager for Bluetooth Low Energy. Responsible for scanning and creating connections. Filters can be used for setting Bluetooth specific parameters.
Macros#
#define
BLE_PEER_MANAGER_CENTRAL_CONFIG_DEFAULT_SCANNING_PHY sl_bt_gap_phy_coding_1m_uncoded
#define
BLE_PEER_MANAGER_CENTRAL_CONFIG_DEFAULT_SCAN_DISCOVERY_MODE sl_bt_scanner_discover_generic
#define
BLE_PEER_MANAGER_CENTRAL_CONFIG_DEFAULT_SCAN_MODE sl_bt_scanner_scan_mode_passive
Macro Definition Documentation#
BLE_PEER_MANAGER_CENTRAL_CONFIG_DEFAULT_SCANNING_PHY#
#define BLE_PEER_MANAGER_CENTRAL_CONFIG_DEFAULT_SCANNING_PHYValue:
sl_bt_gap_phy_coding_1m_uncoded
BLE_PEER_MANAGER_CENTRAL_CONFIG_DEFAULT_SCAN_DISCOVERY_MODE#
#define BLE_PEER_MANAGER_CENTRAL_CONFIG_DEFAULT_SCAN_DISCOVERY_MODEValue:
sl_bt_scanner_discover_generic
BLE_PEER_MANAGER_CENTRAL_CONFIG_DEFAULT_SCAN_MODE#
#define BLE_PEER_MANAGER_CENTRAL_CONFIG_DEFAULT_SCAN_MODEValue:
sl_bt_scanner_scan_mode_passive
BLE_PEER_MANAGER_CENTRAL_CONFIG_DEFAULT_SCAN_INTERVAL#
#define BLE_PEER_MANAGER_CENTRAL_CONFIG_DEFAULT_SCAN_INTERVALValue:
16
BLE_PEER_MANAGER_CENTRAL_CONFIG_DEFAULT_SCAN_WINDOW#
#define BLE_PEER_MANAGER_CENTRAL_CONFIG_DEFAULT_SCAN_WINDOWValue:
16