GATT Descriptor Property Flags#

This enum defines the property flags for GATT characteristic descriptors.

Macros#

#define

A GATT client can read the descriptor value.

#define

A GATT client can write the descriptor value.

#define

A GATT client can write the descriptor value without a response.

#define

The descriptor is local only and should be invisible to GATT clients.

Macro Definition Documentation#

SL_BT_GATTDB_DESCRIPTOR_READ#

#define SL_BT_GATTDB_DESCRIPTOR_READ
Value:
0x1

A GATT client can read the descriptor value.


SL_BT_GATTDB_DESCRIPTOR_WRITE#

#define SL_BT_GATTDB_DESCRIPTOR_WRITE
Value:
0x2

A GATT client can write the descriptor value.


SL_BT_GATTDB_DESCRIPTOR_WRITE_NO_RESPONSE#

#define SL_BT_GATTDB_DESCRIPTOR_WRITE_NO_RESPONSE
Value:
0x4

A GATT client can write the descriptor value without a response.


SL_BT_GATTDB_DESCRIPTOR_LOCAL_ONLY#

#define SL_BT_GATTDB_DESCRIPTOR_LOCAL_ONLY
Value:
0x200

The descriptor is local only and should be invisible to GATT clients.