Periodic Advertising Configuration Flags#

Defines configuration flags for periodic advertising.

Macros#

#define

Include the TX power in advertising packets.

#define

Automatically start the extended advertising on the advertising set. The advertising will be started in non-connectable and non-scannable mode.

#define

Include Advertising Data Information (ADI) field in periodic advertising PDUs.

Macro Definition Documentation#

SL_BT_PERIODIC_ADVERTISER_INCLUDE_TX_POWER#

#define SL_BT_PERIODIC_ADVERTISER_INCLUDE_TX_POWER
Value:
0x1

Include the TX power in advertising packets.


SL_BT_PERIODIC_ADVERTISER_AUTO_START_EXTENDED_ADVERTISING#

#define SL_BT_PERIODIC_ADVERTISER_AUTO_START_EXTENDED_ADVERTISING
Value:
0x2

Automatically start the extended advertising on the advertising set. The advertising will be started in non-connectable and non-scannable mode.


SL_BT_PERIODIC_ADVERTISER_INCLUDE_ADVERTISING_DATA_INFORMATION#

#define SL_BT_PERIODIC_ADVERTISER_INCLUDE_ADVERTISING_DATA_INFORMATION
Value:
0x4

Include Advertising Data Information (ADI) field in periodic advertising PDUs.