Connection Management (le_connection)#

The commands and events in this class are related to managing connection establishment, parameter setting, and disconnection procedures.

le_connection commands#

le_connection_close#

Close a Bluetooth connection or cancel an ongoing connection establishment process. The parameter is a connection handle which is reported in le_connection_opened event or le_gap_connect response.

C API#

/* Function */
struct gecko_msg_le_connection_close_rsp_t *gecko_cmd_le_connection_close(uint8 connection);

/* Response id */
gecko_rsp_le_connection_close_id

/* Response structure */
struct gecko_msg_le_connection_close_rsp_t
{
  uint16 result;
}

Command Parameters (for BGAPI headers refer to link)#

Type

Name

Description

uint8

connection

Handle of the connection to be closed

Response Parameters (for BGAPI headers refer to link)#

Type

Name

Description

uint16

result

Result code

  • 0: success

  • Non-zero: an error occurred
    For other values refer to the Error codes

Events generated#

Event

Description

le_connection_closed

le_connection_disable_slave_latency#

Temporarily enable or disable slave latency. Used only when Bluetooth device is acting as slave. When slave latency is disabled, the slave latency connection parameter is not set to 0 but the device will wake up on every connection interval to receive and send packets.

C API#

/* Function */
struct gecko_msg_le_connection_disable_slave_latency_rsp_t *gecko_cmd_le_connection_disable_slave_latency(uint8 connection, uint8 disable);

/* Response id */
gecko_rsp_le_connection_disable_slave_latency_id

/* Response structure */
struct gecko_msg_le_connection_disable_slave_latency_rsp_t
{
  uint16 result;
}

Command Parameters (for BGAPI headers refer to link)#

Type

Name

Description

uint8

connection

Connection Handle

uint8

disable

0 enable, 1 disable slave latency. Default: 0

Response Parameters (for BGAPI headers refer to link)#

Type

Name

Description

uint16

result

Result code

  • 0: success

  • Non-zero: an error occurred
    For other values refer to the Error codes

le_connection_get_rssi#

Get the latest RSSI value of a Bluetooth connection. The RSSI value will be reported in a le_connection_rssi event.

C API#

/* Function */
struct gecko_msg_le_connection_get_rssi_rsp_t *gecko_cmd_le_connection_get_rssi(uint8 connection);

/* Response id */
gecko_rsp_le_connection_get_rssi_id

/* Response structure */
struct gecko_msg_le_connection_get_rssi_rsp_t
{
  uint16 result;
}

Command Parameters (for BGAPI headers refer to link)#

Type

Name

Description

uint8

connection

Connection handle

Response Parameters (for BGAPI headers refer to link)#

Type

Name

Description

uint16

result

Result code

  • 0: success

  • Non-zero: an error occurred
    For other values refer to the Error codes

Events generated#

Event

Description

le_connection_rssi

Triggered when this command has completed.

le_connection_read_channel_map#

Read channel map for a specified connection.

C API#

/* Function */
struct gecko_msg_le_connection_read_channel_map_rsp_t *gecko_cmd_le_connection_read_channel_map(uint8 connection);

/* Response id */
gecko_rsp_le_connection_read_channel_map_id

/* Response structure */
struct gecko_msg_le_connection_read_channel_map_rsp_t
{
  uint16 result;
  uint8array channel_map;
}

Command Parameters (for BGAPI headers refer to link)#

Type

Name

Description

uint8

connection

Connection Handle

Response Parameters (for BGAPI headers refer to link)#

Type

Name

Description

uint16

result

Result code

  • 0: success

  • Non-zero: an error occurred
    For other values refer to the Error codes

uint8array

channel_map

This parameter is 5 bytes and contains 37 1-bit fields.
The nth field (in the range 0 to 36) contains the value for the link layer channel index n.

  • 0: Channel n is unused.

  • 1: Channel n is used.

The most significant bits are reserved for future use.

le_connection_set_parameters#

Deprecated and replaced by le_connection_set_timing_parameters command.

Request a change in the connection parameters of a Bluetooth connection.

C API#

/* Function */
struct gecko_msg_le_connection_set_parameters_rsp_t *gecko_cmd_le_connection_set_parameters(uint8 connection, uint16 min_interval, uint16 max_interval, uint16 latency, uint16 timeout);

/* Response id */
gecko_rsp_le_connection_set_parameters_id

/* Response structure */
struct gecko_msg_le_connection_set_parameters_rsp_t
{
  uint16 result;
}

Command Parameters (for BGAPI headers refer to link)#

Type

Name

Description

uint8

connection

Connection Handle

uint16

min_interval

Minimum value for the connection event interval.

This must be set be less than or equal to max_interval.

  • Time = Value x 1.25 ms

  • Range: 0x0006 to 0x0c80

  • Time Range: 7.5 ms to 4 s

uint16

max_interval

Maximum value for the connection event interval. This must be set greater than or equal to min_interval.

  • Time = Value x 1.25 ms

  • Range: 0x0006 to 0x0c80

  • Time Range: 7.5 ms to 4 s

uint16

latency

Slave latency, which defines how many connection intervals the slave can skip if it has no data to send

  • Range: 0x0000 to 0x01f4

Use 0x0000 for default value

uint16

timeout

Supervision timeout, which defines the time that the connection is maintained although the devices can't communicate at the currently configured connection intervals.

  • Range: 0x000a to 0x0c80

  • Time = Value x 10 ms

  • Time Range: 100 ms to 32 s

  • The value in milliseconds must be larger than (1 + latency) max_interval 2, where max_interval is given in milliseconds

Set the supervision timeout at a value which allows communication attempts over at least a few connection intervals.

Response Parameters (for BGAPI headers refer to link)#

Type

Name

Description

uint16

result

Result code

  • 0: success

  • Non-zero: an error occurred
    For other values refer to the Error codes

Events generated#

Event

Description

le_connection_parameters

Triggered after new connection parameters are applied on the connection.

le_connection_set_phy#

Deprecated and replaced by le_connection_set_preferred_phy command.

Set preferred PHYs for a connection. Preferred PHYs are connection-specific. Event le_connection_phy_status is received when PHY update procedure is completed. Non-preferred PHY can also be set if remote device does not accept any of the preferred PHYs.

NOTE: 2 Mbit and Coded PHYs are not supported by all devices.

C API#

/* Function */
struct gecko_msg_le_connection_set_phy_rsp_t *gecko_cmd_le_connection_set_phy(uint8 connection, uint8 phy);

/* Response id */
gecko_rsp_le_connection_set_phy_id

/* Response structure */
struct gecko_msg_le_connection_set_phy_rsp_t
{
  uint16 result;
}

Command Parameters (for BGAPI headers refer to link)#

Type

Name

Description

uint8

connection

uint8

phy

Preferred PHYs for connection. This parameter is a bitfield

and multiple PHYs can be preferred by setting multiple bits.

  • 0x01: 1M PHY

  • 0x02: 2M PHY

  • 0x04: 125k Coded PHY (S=8)

  • 0x08: 500k Coded PHY (S=2)

Response Parameters (for BGAPI headers refer to link)#

Type

Name

Description

uint16

result

Result code

  • 0: success

  • Non-zero: an error occurred
    For other values refer to the Error codes

Events generated#

Event

Description

le_connection_phy_status

le_connection_set_preferred_phy#

Sets preferred and accepted PHYs for the given connection. Event le_connection_phy_status is received when PHY update procedure is completed. Non-preferred PHY can also be set if remote device does not accept any of the preferred PHYs.

The parameter accepted_phy is used for specifying the PHYs that the stack can accept in a remote initiated PHY update request. A PHY update will not occur if none of the accepted PHYs presents in the request.

NOTE: 2M and Coded PHYs are not supported by all devices.

C API#

/* Function */
struct gecko_msg_le_connection_set_preferred_phy_rsp_t *gecko_cmd_le_connection_set_preferred_phy(uint8 connection, uint8 preferred_phy, uint8 accepted_phy);

/* Response id */
gecko_rsp_le_connection_set_preferred_phy_id

/* Response structure */
struct gecko_msg_le_connection_set_preferred_phy_rsp_t
{
  uint16 result;
}

Command Parameters (for BGAPI headers refer to link)#

Type

Name

Description

uint8

connection

Connection handle

uint8

preferred_phy

Preferred PHYs. This parameter is a bitfield and multiple PHYs can be set.

  • 0x01: 1M PHY

  • 0x02: 2M PHY

  • 0x04: 125k Coded PHY (S=8)

  • 0x08: 500k Coded PHY (S=2)

Default: 0xff (no preference)

uint8

accepted_phy

Accepted PHYs in remotely-initiated PHY update requests. This parameter is a bitfield and multiple PHYs can be set.

  • 0x01: 1M PHY

  • 0x02: 2M PHY

  • 0x04: Coded PHY

  • 0xff: Any PHYs

Default: 0xff (all PHYs accepted)

Response Parameters (for BGAPI headers refer to link)#

Type

Name

Description

uint16

result

Result code

  • 0: success

  • Non-zero: an error occurred
    For other values refer to the Error codes

Events generated#

Event

Description

le_connection_phy_status

le_connection_set_timing_parameters#

Request a change in the connection parameters of a Bluetooth connection.

C API#

/* Function */
struct gecko_msg_le_connection_set_timing_parameters_rsp_t *gecko_cmd_le_connection_set_timing_parameters(uint8 connection, uint16 min_interval, uint16 max_interval, uint16 latency, uint16 timeout, uint16 min_ce_length, uint16 max_ce_length);

/* Response id */
gecko_rsp_le_connection_set_timing_parameters_id

/* Response structure */
struct gecko_msg_le_connection_set_timing_parameters_rsp_t
{
  uint16 result;
}

Command Parameters (for BGAPI headers refer to link)#

Type

Name

Description

uint8

connection

Connection Handle

uint16

min_interval

Minimum value for the connection event interval. This must be set less than or equal to max_interval.

  • Time = Value x 1.25 ms

  • Range: 0x0006 to 0x0c80

  • Time Range: 7.5 ms to 4 s

uint16

max_interval

Maximum value for the connection event interval. This must be set greater than or equal to min_interval.

  • Time = Value x 1.25 ms

  • Range: 0x0006 to 0x0c80

  • Time Range: 7.5 ms to 4 s

uint16

latency

Slave latency, which defines how many connection intervals the slave can skip if it has no data to send

  • Range: 0x0000 to 0x01f4

Use 0x0000 for default value

uint16

timeout

Supervision timeout, which defines the time that the connection is maintained although the devices can't communicate at the currently configured connection intervals.

  • Range: 0x000a to 0x0c80

  • Time = Value x 10 ms

  • Time Range: 100 ms to 32 s

  • The value in milliseconds must be larger than (1 + latency) max_interval 2, where max_interval is given in milliseconds

Set the supervision timeout at a value which allows communication attempts over at least a few connection intervals.

uint16

min_ce_length

Minimum value for the connection event length. This must be set less than or equal to max_ce_length.

  • Time = Value x 0.625 ms

  • Range: 0x0000 to 0xffff

Value is not currently used and is reserved for future. Set to 0.

uint16

max_ce_length

Maximum value for the connection event length. This must be set greater than or equal to min_ce_length.

  • Time = Value x 0.625 ms

  • Range: 0x0000 to 0xffff

Use 0xffff for no limitation.

Response Parameters (for BGAPI headers refer to link)#

Type

Name

Description

uint16

result

Result code

  • 0: success

  • Non-zero: an error occurred
    For other values refer to the Error codes

Events generated#

Event

Description

le_connection_parameters

Triggered after new connection parameters are applied on the connection.

le_connection events#

le_connection_opened#

Indicates that a new connection was opened. This event does not indicate that the connection was established (i.e., that a data packet was received within 6 connection interval). If the connection does not get established, an le_connection_closed event may immediately follow. This event also reports whether the connected devices are already bonded, and what the role of the Bluetooth device (Slave or Master) is. An open connection can be closed with the le_connection_close command by giving the connection handle obtained from this event.

C API#

/* event id*/
gecko_evt_le_connection_opened_id

/* event structure*/
struct gecko_msg_le_connection_opened_evt_t
{
  bd_addr address;
  uint8 address_type;
  uint8 master;
  uint8 connection;
  uint8 bonding;
  uint8 advertiser;
}

Event Parameters (for BGAPI headers refer to link)#

Type

Name

Description

bd_addr

address

Remote device address

uint8

address_type

Remote device address type

uint8

master

Device role in connection. Values:

  • 0: Slave

  • 1: Master

uint8

connection

Handle for new connection

uint8

bonding

Bonding handle. Values:

  • 0xff: No bonding

  • Other: Bonding handle

uint8

advertiser

The local advertising set that this connection was opened to. Values:

  • 0xff: Invalid value or not applicable. Ignore this field

  • Other: The advertising set handle

le_connection_closed#

Indicates that a connection was closed.

C API#

/* event id*/
gecko_evt_le_connection_closed_id

/* event structure*/
struct gecko_msg_le_connection_closed_evt_t
{
  uint16 reason;
  uint8 connection;
}

Event Parameters (for BGAPI headers refer to link)#

Type

Name

Description

uint16

reason

Result code

  • 0: success

  • Non-zero: an error occurred
    For other values refer to the Error codes

uint8

connection

Handle of the closed connection

le_connection_parameters#

Triggered whenever the connection parameters are changed and at any time a connection is established.

C API#

/* event id*/
gecko_evt_le_connection_parameters_id

/* event structure*/
struct gecko_msg_le_connection_parameters_evt_t
{
  uint8 connection;
  uint16 interval;
  uint16 latency;
  uint16 timeout;
  uint8 security_mode;
  uint16 txsize;
}

Event Parameters (for BGAPI headers refer to link)#

Type

Name

Description

uint8

connection

Connection handle

uint16

interval

Connection interval. Time = Value x 1.25 ms

uint16

latency

Slave latency (how many connection intervals the slave can skip)

uint16

timeout

Supervision timeout. Time = Value x 10 ms

uint8

security_mode

Connection security mode

uint16

txsize

Maximum Data Channel PDU Payload size that the controller can send in an air packet

le_connection_rssi#

Triggered when an le_connection_get_rssi command has completed.

C API#

/* event id*/
gecko_evt_le_connection_rssi_id

/* event structure*/
struct gecko_msg_le_connection_rssi_evt_t
{
  uint8 connection;
  uint8 status;
  int8 rssi;
}

Event Parameters (for BGAPI headers refer to link)#

Type

Name

Description

uint8

connection

Connection handle

uint8

status

Command complete status:

  • 0x00: The command succeeded

  • 0x01-0xFF: The command failed. See Bluetooth Core specification v5.0 [Vol 2] Part D, Error Codes

int8

rssi

RSSI in the latest received packet of the connection. Units: dBm. Range: -127 to +20. Ignore this parameter if the command fails.

le_connection_phy_status#

Indicates that PHY update procedure is completed.

C API#

/* event id*/
gecko_evt_le_connection_phy_status_id

/* event structure*/
struct gecko_msg_le_connection_phy_status_evt_t
{
  uint8 connection;
  uint8 phy;
}

Event Parameters (for BGAPI headers refer to link)#

Type

Name

Description

uint8

connection

Connection handle

uint8

phy

Current active PHY. See values from le_connection_set_preferred_phy command.

le_connection enumerations#

le_connection_security#

Indicate the Bluetooth Security Mode.

Enumerations#

Value

Name

Description

0

le_connection_mode1_level1

No security

1

le_connection_mode1_level2

Unauthenticated pairing with encryption

2

le_connection_mode1_level3

Authenticated pairing with encryption

3

le_connection_mode1_level4

Authenticated Secure Connections pairing with encryption using a 128-bit strength encryption key