Periodic Advertising Synchronization (sync)#

Provides periodic advertising synchronization feature.

When this feature is used, enable event le_gap_extended_scan_response which contains useful information for establishing a synchronization.

sync commands#

sync_close#

Closes a periodic advertising synchronization or cancels an ongoing attempt of establishing a synchronization.

C API#

/* Function */
struct gecko_msg_sync_close_rsp_t *gecko_cmd_sync_close(uint8 sync);

/* Response id */
gecko_rsp_sync_close_id

/* Response structure */
struct gecko_msg_sync_close_rsp_t
{
  uint16 result;
}

Command Parameters (for BGAPI headers refer to link)#

Type

Name

Description

uint8

sync

Periodic advertising synchronization handle

Response Parameters (for BGAPI headers refer to link)#

Type

Name

Description

uint16

result

Result code

  • 0: success

  • Non-zero: an error occurred
    For other values refer to the Error codes

Events generated#

Event

Description

sync_closed

Triggered after a periodic advertising synchronization has been closed or canceled.

sync_open#

Establish a synchronization with a periodic advertising from the specified advertiser and begin receiving periodic advertising packets. Note that synchronization establishment can only occur when scanning is enabled. While scanning is disabled, no attempt to synchronize will occur.

The application should determine skip and timeout values based on the periodic advertising interval provided by the advertiser. If skip and timeout are used, select appropriate values so that they allow a few receiving attempts. Periodic advertising intervals are reported in event le_gap_extended_scan_response.

C API#

/* Function */
struct gecko_msg_sync_open_rsp_t *gecko_cmd_sync_open(uint8 adv_sid, uint16 skip, uint16 timeout, bd_addr address, uint8 address_type);

/* Response id */
gecko_rsp_sync_open_id

/* Response structure */
struct gecko_msg_sync_open_rsp_t
{
  uint16 result;
  uint8 sync;
}

Command Parameters (for BGAPI headers refer to link)#

Type

Name

Description

uint8

adv_sid

Advertising set identifier

uint16

skip

The maximum number of periodic advertising packets that can be skipped after a successful receive. Range: 0x0000 to 0x01F3

uint16

timeout

The maximum permitted time between successful receives. If this time is exceeded, synchronization is lost. Unit: 10 ms.

  • Range: 0x06 to 0xFFFF

  • Unit: 10 ms

  • Time range: 100 ms ms to 163.84 s

bd_addr

address

Address of the advertiser

uint8

address_type

Advertiser address type. Values:

  • 0: Public address

  • 1: Random address

Response Parameters (for BGAPI headers refer to link)#

Type

Name

Description

uint16

result

Result code

  • 0: success

  • Non-zero: an error occurred
    For other values refer to the Error codes

uint8

sync

A handle that will be assigned to the periodic advertising synchronization after the synchronization is established. This handle is valid only if the result code of this response is 0 (zero).

Events generated#

Event

Description

sync_opened

Triggered after the synchronization is established.

sync_data

Indicates that a periodic advertisement packet is received.

sync events#

sync_opened#

Indicates that a periodic advertising synchronization has been opened.

C API#

/* event id*/
gecko_evt_sync_opened_id

/* event structure*/
struct gecko_msg_sync_opened_evt_t
{
  uint8 sync;
  uint8 adv_sid;
  bd_addr address;
  uint8 address_type;
  uint8 adv_phy;
  uint16 adv_interval;
  uint16 clock_accuracy;
}

Event Parameters (for BGAPI headers refer to link)#

Type

Name

Description

uint8

sync

Periodic advertising synchronization handle

uint8

adv_sid

Advertising set identifier

bd_addr

address

Address of the advertiser

uint8

address_type

Advertiser address type. Values:

  • 0: Public address

  • 1: Random address

uint8

adv_phy

The advertiser PHY. Value:

  • 1: 1M PHY

  • 2: 2M PHY

  • 4: Coded PHY

uint16

adv_interval

The periodic advertising interval. Value in units of 1.25 ms

  • Range: 0x06 to 0xFFFF

  • Time range: 7.5 ms to 81.92 s

uint16

clock_accuracy

The advertiser clock accuracy.

sync_closed#

Indicates that a periodic advertising synchronization lost or a synchronization establishment procedure was canceled.

C API#

/* event id*/
gecko_evt_sync_closed_id

/* event structure*/
struct gecko_msg_sync_closed_evt_t
{
  uint16 reason;
  uint8 sync;
}

Event Parameters (for BGAPI headers refer to link)#

Type

Name

Description

uint16

reason

Result code

  • 0: success

  • Non-zero: an error occurred
    For other values refer to the Error codes

uint8

sync

Periodic advertising synchronization handle

sync_data#

Reports a received periodic advertisement packet.

C API#

/* event id*/
gecko_evt_sync_data_id

/* event structure*/
struct gecko_msg_sync_data_evt_t
{
  uint8 sync;
  int8 tx_power;
  int8 rssi;
  uint8 data_status;
  uint8array data;
}

Event Parameters (for BGAPI headers refer to link)#

Type

Name

Description

uint8

sync

Periodic advertising synchronization handle

int8

tx_power

TX power value in the received packet header. Units: dBm

  • Valid value range: -127 to 126

  • Value 127: information unavailable

int8

rssi

Signal strength indicator (RSSI) in the latest received packet. Units: dBm

  • Range: -127 to +20

uint8

data_status

Data completeness:

  • 0: Complete

  • 1: Incomplete, more data to come in new events

  • 2: Incomplete, data truncated, no more to come

uint8array

data

Periodic advertising data

sync enumerations#

sync_advertiser_clock_accuracy#

These values indicate the advertiser clock accuracy in a periodic advertising synchronization.

Enumerations#

Value

Name

Description

500

sync_clock_accuracy_500

Clock accuracy 500 ppm

250

sync_clock_accuracy_250

Clock accuracy 250 ppm

150

sync_clock_accuracy_150

Clock accuracy 150 ppm

100

sync_clock_accuracy_100

Clock accuracy 100 ppm

75

sync_clock_accuracy_75

Clock accuracy 75 ppm

50

sync_clock_accuracy_50

Clock accuracy 50 ppm

30

sync_clock_accuracy_30

Clock accuracy 30 ppm

20

sync_clock_accuracy_20

Clock accuracy 20 ppm