Endpoint (endpoint)#
This class provides a command for closing Bluetooth connections.
endpoint commands#
endpoint_close#
Deprecated. Use new command le_connection_close to close Bluetooth connections.
This command can be used to close a Bluetooth connection. The parameter is a connection handle which is reported in event le_connection_opened.
Command#
Byte | Type | Name | Description |
|---|---|---|---|
0 | 0x20 | hilen | Message type: Command |
1 | 0x01 | lolen | Minimum payload length |
2 | 0x0b | class | Message class:Endpoint |
3 | 0x02 | method | Message ID |
4 | uint8 | endpoint | The connection handle |
Response#
Byte | Type | Name | Description |
|---|---|---|---|
0 | 0x20 | hilen | Message type: Response |
1 | 0x03 | lolen | Minimum payload length |
2 | 0x0b | class | Message class:Endpoint |
3 | 0x02 | method | Message ID |
4-5 | uint16 | result | Result code |
0: success
Non-zero: an error occurred
For other values refer to the Error codes
6 | uint8 | endpoint | The connection handle that was closed
API#
/* Function */
struct gecko_msg_endpoint_close_rsp_t *gecko_cmd_endpoint_close(uint8 endpoint);
/* Response id */
gecko_rsp_endpoint_close_id
/* Response structure */
struct gecko_msg_endpoint_close_rsp_t
{
uint16 result,
uint8 endpoint
} Events generated#
Event | Description |
|---|---|
le_connection_closed |