Connection management (le_connection)#

The commands and events in this class are related to managing connection establishment, parameter setting, and disconnection procedures.

Commands#

le_connection_close#

This command can be used to close a Bluetooth connection or cancel an ongoing connection establishment process. The parameter is a connection handle which is reported in le_connection_opened event or le_gap_open response.

Command#

Byte

Type

Name

Description

0

0x20

hilen

Message type: Command

1

0x01

lolen

Minimum payload length

2

0x08

class

Message class:Connection management

3

0x04

method

Message ID

4

uint8

connection

Handle of the connection to be closed

Response#

Byte

Type

Name

Description

0

0x20

hilen

Message type: Response

1

0x02

lolen

Minimum payload length

2

0x08

class

Message class:Connection management

3

0x04

method

Message ID

4-5

uint16

result

Result code:

  • 0: success

  • Non-zero: an error occurred

For other values refer to the Error codes

API#

/* Function */
struct gecko_msg_le_connection_close_rsp_t *gecko_cmd_le_connection_close(uint8 connection);

/* Response id */
gecko_rsp_le_connection_close_id

/* Response structure */
struct gecko_msg_le_connection_close_rsp_t
{
  uint16 result
}

Events generated#

Event

Description

le_connection_closed

le_connection_disable_slave_latency#

This command temporarily enables or disables slave latency. Used only when Bluetooth device is in slave role.

Command#

Byte

Type

Name

Description

0

0x20

hilen

Message type: Command

1

0x02

lolen

Minimum payload length

2

0x08

class

Message class:Connection management

3

0x02

method

Message ID

4

uint8

connection

Connection Handle

5

uint8

disable

0 enable, 1 disable slave latency

Response#

Byte

Type

Name

Description

0

0x20

hilen

Message type: Response

1

0x02

lolen

Minimum payload length

2

0x08

class

Message class:Connection management

3

0x02

method

Message ID

4-5

uint16

result

Result code:

  • 0: success

  • Non-zero: an error occurred

For other values refer to the Error codes

API#

/* Function */
struct gecko_msg_le_connection_disable_slave_latency_rsp_t *gecko_cmd_le_connection_disable_slave_latency(uint8 connection, uint8 disable);

/* Response id */
gecko_rsp_le_connection_disable_slave_latency_id

/* Response structure */
struct gecko_msg_le_connection_disable_slave_latency_rsp_t
{
  uint16 result
}

le_connection_get_rssi#

This command can be used to get the latest RSSI value of a Bluetooth connection.

Command#

Byte

Type

Name

Description

0

0x20

hilen

Message type: Command

1

0x01

lolen

Minimum payload length

2

0x08

class

Message class:Connection management

3

0x01

method

Message ID

4

uint8

connection

Connection handle

Response#

Byte

Type

Name

Description

0

0x20

hilen

Message type: Response

1

0x02

lolen

Minimum payload length

2

0x08

class

Message class:Connection management

3

0x01

method

Message ID

4-5

uint16

result

Result code:

  • 0: success

  • Non-zero: an error occurred

For other values refer to the Error codes

API#

/* Function */
struct gecko_msg_le_connection_get_rssi_rsp_t *gecko_cmd_le_connection_get_rssi(uint8 connection);

/* Response id */
gecko_rsp_le_connection_get_rssi_id

/* Response structure */
struct gecko_msg_le_connection_get_rssi_rsp_t
{
  uint16 result
}

Events generated#

Event

Description

le_connection_rssi

Triggered when this command has completed.

le_connection_set_parameters#

This command can be used to request a change in the connection parameters of a Bluetooth connection.

Command#

Byte

Type

Name

Description

0

0x20

hilen

Message type: Command

1

0x09

lolen

Minimum payload length

2

0x08

class

Message class:Connection management

3

0x00

method

Message ID

4

uint8

connection

Connection Handle

5-6

uint16

min_interval

Minimum value for the connection event interval. This must be set be less than or equal to max_interval.

  • Time = Value x 1.25 ms

  • Range: 0x0006 to 0x0c80

  • Time Range: 7.5 ms to 4 s

7-8

uint16

max_interval

Maximum value for the connection event interval. This must be set greater than or equal to min_interval.

  • Time = Value x 1.25 ms

  • Range: 0x0006 to 0x0c80

  • Time Range: 7.5 ms to 4 s

9-10

uint16

latency

Slave latency. This parameter defines how many connection intervals the slave can skip if it has no data to send

  • Range: 0x0000 to 0x01f4

Use 0x0000 for default value

11-12

uint16

timeout

Supervision timeout. The supervision timeout defines for how long the connection is maintained despite the devices being unable to communicate at the currently configured connection intervals.

  • Range: 0x000a to 0x0c80

  • Time = Value x 10 ms

  • Time Range: 100 ms to 32 s

  • The value in milliseconds must be larger than (1 + latency) max_interval 2, where max_interval is given in milliseconds

It is recommended that the supervision timeout is set at a value which allows communication attempts over at least a few connection intervals.

Response#

Byte

Type

Name

Description

0

0x20

hilen

Message type: Response

1

0x02

lolen

Minimum payload length

2

0x08

class

Message class:Connection management

3

0x00

method

Message ID

4-5

uint16

result

Result code:

  • 0: success

  • Non-zero: an error occurred

For other values refer to the Error codes

API#

/* Function */
struct gecko_msg_le_connection_set_parameters_rsp_t *gecko_cmd_le_connection_set_parameters(uint8 connection, uint16 min_interval, uint16 max_interval, uint16 latency, uint16 timeout);

/* Response id */
gecko_rsp_le_connection_set_parameters_id

/* Response structure */
struct gecko_msg_le_connection_set_parameters_rsp_t
{
  uint16 result
}

Events generated#

Event

Description

le_connection_parameters

This event is triggered after new connection parameters has been applied on the connection.

le_connection_set_phy#

This command can be used to set preferred PHYs for connection. Preferred PHYs are connection specific. Event le_connection_phy_status is received when PHY update procedure has been completed. Other than preferred PHY can also be set if remote device does not accept any of the preferred PHYs.

NOTE: 2 Mbit and Coded PHYs are not supported by all devices.

Command#

Byte

Type

Name

Description

0

0x20

hilen

Message type: Command

1

0x02

lolen

Minimum payload length

2

0x08

class

Message class:Connection management

3

0x03

method

Message ID

4

uint8

connection

5

uint8

phy

Preferred PHYs for connection. This parameter is bitfield and multiple PHYs can be preferred by setting multiple bits.

  • 0x01: 1 Mbit PHY

  • 0x02: 2 Mbit PHY

  • 0x04: 125 kbit Coded PHY (S=8)

  • 0x08: 500 kbit Coded PHY (S=2)

Response#

Byte

Type

Name

Description

0

0x20

hilen

Message type: Response

1

0x02

lolen

Minimum payload length

2

0x08

class

Message class:Connection management

3

0x03

method

Message ID

4-5

uint16

result

Result code:

  • 0: success

  • Non-zero: an error occurred

For other values refer to the Error codes

API#

/* Function */
struct gecko_msg_le_connection_set_phy_rsp_t *gecko_cmd_le_connection_set_phy(uint8 connection, uint8 phy);

/* Response id */
gecko_rsp_le_connection_set_phy_id

/* Response structure */
struct gecko_msg_le_connection_set_phy_rsp_t
{
  uint16 result
}

Events generated#

Event

Description

le_connection_phy_status

Events#

le_connection_opened#

This event indicates that a new connection was opened, whether the devices are already bonded, and what is the role of the Bluetooth device (Slave or Master). An open connection can be closed with the le_connection_close command by giving the connection handle ID obtained from this event.

Event#

Byte

Type

Name

Description

0

0xa0

hilen

Message type: Event

1

0x0b

lolen

Minimum payload length

2

0x08

class

Message class:Connection management

3

0x00

method

Message ID

4-9

bd_addr

address

Remote device address

10

uint8

address_type

Remote device address type

11

uint8

master

Device role in connection. Values:

  • 0: Slave

  • 1: Master

12

uint8

connection

Handle for new connection

13

uint8

bonding

Bonding handle. Values:

  • 0xff: No bonding

  • Other: Bonding handle

14

uint8

advertiser

The local advertising set this connection was opened to. Values:

  • 0xff: Invalid value or not applicable, and this field should be ignored

  • Other: The advertising set handle

API#

/* event id*/
gecko_evt_le_connection_opened_id

/* event structure*/
struct gecko_msg_le_connection_opened_evt_t
{
  bd_addr address,
  uint8 address_type,
  uint8 master,
  uint8 connection,
  uint8 bonding,
  uint8 advertiser
}

le_connection_closed#

This event indicates that a connection was closed.

Event#

Byte

Type

Name

Description

0

0xa0

hilen

Message type: Event

1

0x03

lolen

Minimum payload length

2

0x08

class

Message class:Connection management

3

0x01

method

Message ID

4-5

uint16

reason

Result code:

  • 0: success

  • Non-zero: an error occurred

For other values refer to the Error codes

6

uint8

connection

Handle of the closed connection

API#

/* event id*/
gecko_evt_le_connection_closed_id

/* event structure*/
struct gecko_msg_le_connection_closed_evt_t
{
  uint16 reason,
  uint8 connection
}

le_connection_parameters#

This event is triggered whenever the connection parameters are changed and at any time a connection is established.

Event#

Byte

Type

Name

Description

0

0xa0

hilen

Message type: Event

1

0x0a

lolen

Minimum payload length

2

0x08

class

Message class:Connection management

3

0x02

method

Message ID

4

uint8

connection

Connection handle

5-6

uint16

interval

Connection interval

7-8

uint16

latency

Slave latency

9-10

uint16

timeout

Supervision timeout

11

uint8

security_mode

Connection security mode

12-13

uint16

txsize

Maximum Data Channel PDU Payload size the controller can send in an air packet

API#

/* event id*/
gecko_evt_le_connection_parameters_id

/* event structure*/
struct gecko_msg_le_connection_parameters_evt_t
{
  uint8 connection,
  uint16 interval,
  uint16 latency,
  uint16 timeout,
  uint8 security_mode,
  uint16 txsize
}

le_connection_rssi#

This event is triggered when an le_connection_get_rssi command has completed.

Event#

Byte

Type

Name

Description

0

0xa0

hilen

Message type: Event

1

0x03

lolen

Minimum payload length

2

0x08

class

Message class:Connection management

3

0x03

method

Message ID

4

uint8

connection

Connection handle

5

uint8

status

Command complete status:

  • 0x00: The command succeeded

  • 0x01-0xFF: The command failed. See Bluetooth Core specification v5.0 [Vol 2] Part D, Error Codes

6

int8

rssi

RSSI in the latest received packet of the connection. This parameter should be ignored if the command failed. Range: -127 to +20. Units: dBm.

API#

/* event id*/
gecko_evt_le_connection_rssi_id

/* event structure*/
struct gecko_msg_le_connection_rssi_evt_t
{
  uint8 connection,
  uint8 status,
  int8 rssi
}

le_connection_phy_status#

This event indicates that PHY update procedure has been completed.

Event#

Byte

Type

Name

Description

0

0xa0

hilen

Message type: Event

1

0x02

lolen

Minimum payload length

2

0x08

class

Message class:Connection management

3

0x04

method

Message ID

4

uint8

connection

5

uint8

phy

Current active PHY. See values from le_connection_set_phy command.

API#

/* event id*/
gecko_evt_le_connection_phy_status_id

/* event structure*/
struct gecko_msg_le_connection_phy_status_evt_t
{
  uint8 connection,
  uint8 phy
}

Enumerations#

le_connection_security#

These values indicate the Bluetooth Security Mode.

Enumerations#

Value

Name

Description

0

le_connection_mode1_level1

No security

1

le_connection_mode1_level2

Unauthenticated pairing with encryption

2

le_connection_mode1_level3

Authenticated pairing with encryption

3

le_connection_mode1_level4

Authenticated Secure Connections pairing with encryption using a 128-bit strength encryption key