sl_bt_evt_advertiser_scan_requestAdvertiser#
Reports any scan request received in advertising mode if the scan request notification is enabled.
Data Structures#
struct sl_bt_evt_advertiser_scan_request_s
Data structure of the scan_request event.
Macros#
#define sl_bt_evt_advertiser_scan_request_id 0x020400a0
Identifier of the scan_request event.
Detailed Description#
Reports any scan request received in advertising mode if the scan request notification is enabled.
Do not confuse this event with the scan response.
Data Structure Documentation#
sl_bt_evt_advertiser_scan_request_s#
struct sl_bt_evt_advertiser_scan_request_s |
Data structure of the scan_request event.
Data Fields | ||
|---|---|---|
uint8_t | handle | Advertising set handle where scan request was received |
address | Bluetooth address of the scanning device | |
uint8_t | address_type | Scanner address type. Values:
|
uint8_t | bonding | Bonding handle if the remote scanning device has previously bonded with the local device. Values
|