sl_bt_evt_advertiser_timeoutAdvertiser#
Indicates that the advertiser has completed the configured number of advertising events in the advertising set and advertising has stopped.
Data Structures#
struct sl_bt_evt_advertiser_timeout_s
Data structure of the timeout event.
Macros#
#define sl_bt_evt_advertiser_timeout_id 0x010400a0
Identifier of the timeout event.
Detailed Description#
Indicates that the advertiser has completed the configured number of advertising events in the advertising set and advertising has stopped.
The maximum number of advertising events can be configured by the maxevents parameter in the command sl_bt_advertiser_set_timing.
Data Structure Documentation#
sl_bt_evt_advertiser_timeout_s#
struct sl_bt_evt_advertiser_timeout_s |
Data structure of the timeout event.
Data Fields | ||
|---|---|---|
uint8_t | handle | The advertising set handle |