sl_bt_evt_sm_passkey_requestSecurity Manager#
Indicates a request for the passkey prompt displayed on the remote device.
Data Structures#
struct | sl_bt_evt_sm_passkey_request_s Data structure of the passkey_request event. |
Macros#
#define | sl_bt_evt_sm_passkey_request_id 0x010f00a0 Identifier of the passkey_request event. |
Detailed Description#
Indicates a request for the passkey prompt displayed on the remote device.
Use the command sl_bt_sm_enter_passkey to input the passkey value.
Data Structure Documentation#
sl_bt_evt_sm_passkey_request_s#
struct sl_bt_evt_sm_passkey_request_s
Data structure of the passkey_request event.
Data Fields | ||
|---|---|---|
uint8_t | connection | Connection handle |