sl_bt_evt_dfu_boot_failureDevice Firmware Update#
This event indicates that an error, which prevents the device from booting, has occurred in bootloader.
Data Structures#
struct
Data structure of the boot_failure event.
Macros#
define#
sl_bt_evt_dfu_boot_failure_id 0x010000a0
Identifier of the boot_failure event.
Detailed Description#
This event indicates that an error, which prevents the device from booting, has occurred in bootloader.
Data Structure Documentation#
sl_bt_evt_dfu_boot_failure_s#
struct sl_bt_evt_dfu_boot_failure_s
Data structure of the boot_failure event.
Data Fields
uint16_t
reason
The reason for boot failure.