sl_bt_evt_dfu_bootDevice Firmware Update#
This event indicates that the device booted in DFU mode and is now ready to receive commands related to device firmware upgrade (DFU).
Data Structures#
struct
Data structure of the boot event.
Macros#
#define
sl_bt_evt_dfu_boot_id 0x000000a0
Identifier of the boot event.
Detailed Description#
This event indicates that the device booted in DFU mode and is now ready to receive commands related to device firmware upgrade (DFU).
Data Structure Documentation#
sl_bt_evt_dfu_boot_s#
struct sl_bt_evt_dfu_boot_s
Data structure of the boot event.
Data Fields:
uint32_t
version
The version of the bootloader