sl_bt_evt_connection_parametersConnection#
Triggered whenever the connection parameters are changed and at any time a connection is established.
Data Structures | |
|---|---|
struct | |
Data structure of the parameters event. More... | |
Macros | |
|---|---|
#define | sl_bt_evt_connection_parameters_id 0x020600a0 |
Identifier of the parameters event. | |
Detailed Description#
Triggered whenever the connection parameters are changed and at any time a connection is established.
Data Structure Documentation#
sl_bt_evt_connection_parameters_s#
struct sl_bt_evt_connection_parameters_s
Data structure of the parameters event.
Data Fields | ||
|---|---|---|
uint8_t | connection | Connection handle |
uint16_t | interval | Connection interval. Time = Value x 1.25 ms |
uint16_t | latency | Slave latency (how many connection intervals the slave can skip) |
uint16_t | timeout | Supervision timeout. Time = Value x 10 ms |
uint8_t | security_mode | Enum sl_bt_connection_security_t. Connection security mode. Values:
|
uint16_t | txsize | Maximum Data Channel PDU Payload size that the controller can send in an air packet |