sl_bt_evt_connection_remote_tx_powerConnection#
Reports a transmit power change on the remote device of a connection if transmit power reporting has been enabled.
Data Structures | |
|---|---|
struct | |
Data structure of the remote_tx_power event. More... | |
Macros | |
|---|---|
#define | sl_bt_evt_connection_remote_tx_power_id 0x070600a0 |
Identifier of the remote_tx_power event. | |
Detailed Description#
Reports a transmit power change on the remote device of a connection if transmit power reporting has been enabled.
Enable or disable transmit power reporting using sl_bt_connection_set_power_reporting command.
Data Structure Documentation#
sl_bt_evt_connection_remote_tx_power_s#
struct sl_bt_evt_connection_remote_tx_power_s
Data structure of the remote_tx_power event.
Data Fields | ||
|---|---|---|
uint8_t | connection | Handle of the connection |
uint8_t | phy | Enum sl_bt_gap_phy_and_coding_type_t. The PHY which the transmit power is reported for. Values:
|
int8_t | power_level | Transmit power level. Values:
|
uint8_t | flags | Enum sl_bt_connection_tx_power_flag_t. Transmit power level flags. Ignore this field if
|
int8_t | delta | Change in transmit power level. Values:
|