sl_bt_evt_gatt_mtu_exchangedGATT Client#
Indicates that an ATT_MTU exchange procedure is completed.
Data Structures | |
|---|---|
struct | |
Data structure of the mtu_exchanged event. More... | |
Macros | |
|---|---|
#define | sl_bt_evt_gatt_mtu_exchanged_id 0x000900a0 |
Identifier of the mtu_exchanged event. | |
Detailed Description#
Indicates that an ATT_MTU exchange procedure is completed.
The mtu parameter describes new MTU size. MTU size 23 is used before this event is received.
Data Structure Documentation#
sl_bt_evt_gatt_mtu_exchanged_s#
struct sl_bt_evt_gatt_mtu_exchanged_s
Data structure of the mtu_exchanged event.
Data Fields | ||
|---|---|---|
uint8_t | connection | Connection handle |
uint16_t | mtu | Exchanged ATT_MTU |