sl_bt_evt_gatt_procedure_completedGATT Client#
Indicates that the current GATT procedure was completed successfully or that it failed with an error.
Data Structures | |
|---|---|
struct | |
Data structure of the procedure_completed event. More... | |
Macros | |
|---|---|
#define | sl_bt_evt_gatt_procedure_completed_id 0x060900a0 |
Identifier of the procedure_completed event. | |
Detailed Description#
Indicates that the current GATT procedure was completed successfully or that it failed with an error.
All GATT commands excluding sl_bt_gatt_write_characteristic_value_without_response and sl_bt_gatt_send_characteristic_confirmation will trigger this event. As a result, the application must wait for this event before issuing another GATT command (excluding the two aforementioned exceptions).
Note: After a failed GATT procedure with SL_STATUS_TIMEOUT error, further GATT transactions over this connection are not allowed by the stack.
Data Structure Documentation#
sl_bt_evt_gatt_procedure_completed_s#
struct sl_bt_evt_gatt_procedure_completed_s
Data structure of the procedure_completed event.
Data Fields | ||
|---|---|---|
uint8_t | connection | Connection handle |
uint16_t | result | Result code
|