sl_bt_evt_gatt_server_user_write_requestGATT Server#
Indicates that a remote GATT client is attempting to write a value of an attribute into the local GATT database, where the attribute was defined in the GATT database XML file to have the type="user".
Data Structures | |
|---|---|
struct | |
Data structure of the user_write_request event. More... | |
Macros | |
|---|---|
#define | sl_bt_evt_gatt_server_user_write_request_id 0x020a00a0 |
Identifier of the user_write_request event. | |
Detailed Description#
Indicates that a remote GATT client is attempting to write a value of an attribute into the local GATT database, where the attribute was defined in the GATT database XML file to have the type="user".
The parameter att_opcode informs which attribute procedure was used to write the value. If the att_opcode is sl_bt_gatt_write_request (see sl_bt_gatt_att_opcode_t), the application needs to respond to this request by using the sl_bt_gatt_server_send_user_write_response command within 30 seconds, otherwise further GATT transactions are not allowed by the remote side. If the value of att_opcode is sl_bt_gatt_execute_write_request, it indicates that this is a queued prepare write request received earlier and now the GATT server is processing the execute write. The event sl_bt_evt_gatt_server_execute_write_completed will be emitted after all queued requests have been processed.
Data Structure Documentation#
sl_bt_evt_gatt_server_user_write_request_s#
struct sl_bt_evt_gatt_server_user_write_request_s
Data structure of the user_write_request event.
Data Fields | ||
|---|---|---|
uint8_t | connection | Connection handle |
uint16_t | characteristic | GATT characteristic handle. This value is normally received from the gatt_characteristic event. |
uint8_t | att_opcode | Enum sl_bt_gatt_att_opcode_t. Attribute opcode that informs the procedure from which the value was received. |
uint16_t | offset | Value offset |
value | Value | |