sl_bt_evt_sm_confirm_passkeySecurity Manager#
Indicates a request for passkey display and confirmation by the user.
Data Structures | |
|---|---|
struct | |
Data structure of the confirm_passkey event. | |
Macros | |
|---|---|
#define | sl_bt_evt_sm_confirm_passkey_id 0x020f00a0 |
Identifier of the confirm_passkey event. | |
Detailed Description#
Indicates a request for passkey display and confirmation by the user.
Use the command sl_bt_sm_passkey_confirm to accept or reject the displayed passkey.
Data Structure Documentation#
sl_bt_evt_sm_confirm_passkey_s#
struct sl_bt_evt_sm_confirm_passkey_s
Data structure of the confirm_passkey event.
Data Fields | ||
|---|---|---|
uint8_t | connection | Connection handle |
uint32_t | passkey | Passkey. Range: 0 to 999999.* NOTE! When displaying the passkey to the user, prefix the number with zeros to obtain a 6 digit number
|