sl_bt_evt_sm_bonding_failedSecurity Manager#
This event is triggered if the pairing or bonding procedure fails.
Data Structures | |
|---|---|
struct | |
Data structure of the bonding_failed event. | |
Macros | |
|---|---|
#define | sl_bt_evt_sm_bonding_failed_id 0x040f00a0 |
Identifier of the bonding_failed event. | |
Detailed Description#
This event is triggered if the pairing or bonding procedure fails.
Data Structure Documentation#
sl_bt_evt_sm_bonding_failed_s#
struct sl_bt_evt_sm_bonding_failed_s
Data structure of the bonding_failed event.
Data Fields | ||
|---|---|---|
uint8_t | connection | Connection handle |
uint16_t | reason | Describes error that occurred |