sl_bt_evt_gatt_mtu_exchangedGATT Client#
Indicates that an ATT_MTU exchange procedure is completed.
Data Structures#
struct | sl_bt_evt_gatt_mtu_exchanged_s | Data structure of the mtu_exchanged event.
Macros#
define | sl_bt_evt_gatt_mtu_exchanged_id 0x000900a0#
| Identifier of the mtu_exchanged event.
Detailed Description#
Indicates that an ATT_MTU exchange procedure is completed.
The mtu parameter describes new MTU size. MTU size 23 is used before this
event is received.
Data Structure Documentation#
◆ sl_bt_evt_gatt_mtu_exchanged_s#
struct sl_bt_evt_gatt_mtu_exchanged_s#
Data structure of the mtu_exchanged event.
Data Fields#
uint8_t | connection |
Connection handle
uint16_t | mtu |
Exchanged ATT_MTU