sl_bt_evt_sync_dataSynchronization#

Reports a received periodic advertisement packet.

Data Structures#

struct

sl_bt_evt_sync_data_s

Data structure of the data event.

Macros#

# define

sl_bt_evt_sync_data_id 0x024200a0

Identifier of the data event.

Detailed Description#

Reports a received periodic advertisement packet.


Data Structure Documentation#

◆ sl_bt_evt_sync_data_s#

struct sl_bt_evt_sync_data_s#

Data structure of the data event.

Data Fields

uint16_t

sync

Periodic advertising synchronization handle

int8_t

tx_power

TX power value in the received packet header. Units: dBm

  • Valid value range: -127 to 126

  • Value 127: information unavailable

int8_t

rssi

Signal strength indicator (RSSI) in the latest received packet. Units: dBm

  • Range: -127 to +20

uint8_t

data_status

Data completeness:

  • 0: Complete

  • 1: Incomplete, more data to come in new events

  • 2: Incomplete, data truncated, no more to come

uint8array

data

Periodic advertising data