Testing Commands#

Testing Commands.

Modules#


sl_bt_evt_test_dtm_completed Indicates that the radio has processed a test start or end command.

Enumerations#


enum | sl_bt_test_packet_type_t { sl_bt_test_pkt_prbs9 = 0x0, sl_bt_test_pkt_11110000 = 0x1, sl_bt_test_pkt_10101010 = 0x2, sl_bt_test_pkt_11111111 = 0x4, sl_bt_test_pkt_00000000 = 0x5, sl_bt_test_pkt_00001111 = 0x6, sl_bt_test_pkt_01010101 = 0x7, sl_bt_test_pkt_pn9 = 0xfd, sl_bt_test_pkt_carrier = 0xfe } | Test packet types supported by the stack.

enum | sl_bt_test_phy_t { sl_bt_test_phy_1m = 0x1, sl_bt_test_phy_2m = 0x2, sl_bt_test_phy_125k = 0x3, sl_bt_test_phy_500k = 0x4 } | Test PHY types.

Functions#


SL_BGAPI_DEPRECATED sl_status_t | sl_bt_test_dtm_tx (uint8_t packet_type, uint8_t length, uint8_t channel, uint8_t phy)

sl_status_t | sl_bt_test_dtm_tx_v4 (uint8_t packet_type, uint8_t length, uint8_t channel, uint8_t phy, int8_t power_level)

sl_status_t | sl_bt_test_dtm_rx (uint8_t channel, uint8_t phy)

sl_status_t | sl_bt_test_dtm_end ()

Detailed Description#

Testing Commands.

Enumeration Type Documentation#

◆ sl_bt_test_packet_type_t#

enum sl_bt_test_packet_type_t#

Test packet types supported by the stack.

Enumerator#

sl_bt_test_pkt_prbs9 |

(0x0) PRBS9 packet payload

sl_bt_test_pkt_11110000 |

(0x1) 11110000 packet payload

sl_bt_test_pkt_10101010 |

(0x2) 10101010 packet payload

sl_bt_test_pkt_11111111 |

(0x4) 11111111 packet payload

sl_bt_test_pkt_00000000 |

(0x5) 00000000 packet payload

sl_bt_test_pkt_00001111 |

(0x6) 00001111 packet payload

sl_bt_test_pkt_01010101 |

(0x7) 01010101 packet payload

sl_bt_test_pkt_pn9 |

(0xfd) PN9 continuously modulated output

sl_bt_test_pkt_carrier |

(0xfe) Unmodulated carrier

◆ sl_bt_test_phy_t#

enum sl_bt_test_phy_t#

Test PHY types.

Enumerator#

sl_bt_test_phy_1m |

(0x1) 1M PHY

sl_bt_test_phy_2m |

(0x2) 2M PHY

sl_bt_test_phy_125k |

(0x3) 125k Coded PHY

sl_bt_test_phy_500k |

(0x4) 500k Coded PHY

Function Documentation#

◆ sl_bt_test_dtm_tx()#

SL_BGAPI_DEPRECATED sl_status_t sl_bt_test_dtm_tx

(
	 uint8_t 	 packet_type,
	 uint8_t 	 length,
	 uint8_t 	 channel,
	 uint8_t 	 phy
)

Deprecated and replaced by sl_bt_test_dtm_tx_v4 command.

Start a transmitter test against a separate Bluetooth tester device. When the command is processed by the radio, a sl_bt_evt_test_dtm_completed event is triggered. This event indicates whether the test started successfully.

In the transmitter test, the device sends packets continuously with a fixed interval. The type and length of each packet is set by packet_type and length parameters. The parameter phy specifies which PHY is used to transmit the packets. All devices support at least 1M PHY. A special packet type, test_pkt_carrier, can be used to transmit continuous unmodulated carrier. The length field is ignored in this mode.

The test may be stopped using the sl_bt_test_dtm_end command.

Parameters

 [in]| `packet_type`| Enum [sl_bt_test_packet_type_t](/bluetooth/<docspace-docleaf-version>/bluetooth-commnd-events-testing-commands/#ga5cd6efcb00f31a090c3534f5e08cbdc7). Packet type to transmit. Values:
  • sl_bt_test_pkt_prbs9 (0x0): PRBS9 packet payload

  • sl_bt_test_pkt_11110000 (0x1): 11110000 packet payload

  • sl_bt_test_pkt_10101010 (0x2): 10101010 packet payload

  • sl_bt_test_pkt_11111111 (0x4): 11111111 packet payload

  • sl_bt_test_pkt_00000000 (0x5): 00000000 packet payload

  • sl_bt_test_pkt_00001111 (0x6): 00001111 packet payload

  • sl_bt_test_pkt_01010101 (0x7): 01010101 packet payload

  • sl_bt_test_pkt_pn9 (0xfd): PN9 continuously modulated output

  • sl_bt_test_pkt_carrier (0xfe): Unmodulated carrier

Parameters

[in]| `length`|

Packet length in bytes

Range: 0-255

[in]| `channel`|

Bluetooth channel

Range: 0-39

Channel is (F - 2402) / 2,

where F is frequency in MHz

[in]| `phy`| Enum [sl_bt_test_phy_t](/bluetooth/<docspace-docleaf-version>/bluetooth-commnd-events-testing-commands/#ga35a5e3ed16a6fc6186b45b47565759bc). PHY to use. Values:
  • sl_bt_test_phy_1m (0x1): 1M PHY

  • sl_bt_test_phy_2m (0x2): 2M PHY

  • sl_bt_test_phy_125k (0x3): 125k Coded PHY

  • sl_bt_test_phy_500k (0x4): 500k Coded PHY

Returns

SL_STATUS_OK if successful. Error code otherwise.

Events

◆ sl_bt_test_dtm_tx_v4()#

sl_status_t sl_bt_test_dtm_tx_v4

(
	 uint8_t 	 packet_type,
	 uint8_t 	 length,
	 uint8_t 	 channel,
	 uint8_t 	 phy,
	 int8_t 	 power_level
)

Start a transmitter test against a separate Bluetooth tester device. When the command is processed by the radio, a sl_bt_evt_test_dtm_completed event is triggered. This event indicates whether the test started successfully.

In the transmitter test, the device sends packets continuously with a fixed interval. The type and length of each packet is set by packet_type and length parameters. The parameter phy specifies which PHY is used to transmit the packets. All devices support at least 1M PHY. A special packet type, test_pkt_carrier , can be used to transmit continuous unmodulated carrier. The length field is ignored in this mode.

Stop the test using the sl_bt_test_dtm_end command.

Parameters

 [in]| `packet_type`| Enum [sl_bt_test_packet_type_t](/bluetooth/<docspace-docleaf-version>/bluetooth-commnd-events-testing-commands/#ga5cd6efcb00f31a090c3534f5e08cbdc7). Packet type to transmit. Values:
  • sl_bt_test_pkt_prbs9 (0x0): PRBS9 packet payload

  • sl_bt_test_pkt_11110000 (0x1): 11110000 packet payload

  • sl_bt_test_pkt_10101010 (0x2): 10101010 packet payload

  • sl_bt_test_pkt_11111111 (0x4): 11111111 packet payload

  • sl_bt_test_pkt_00000000 (0x5): 00000000 packet payload

  • sl_bt_test_pkt_00001111 (0x6): 00001111 packet payload

  • sl_bt_test_pkt_01010101 (0x7): 01010101 packet payload

  • sl_bt_test_pkt_pn9 (0xfd): PN9 continuously modulated output

  • sl_bt_test_pkt_carrier (0xfe): Unmodulated carrier

Parameters

[in]| `length`|

Packet length in bytes

Range: 0-255

[in]| `channel`|

Bluetooth channel

Range: 0-39

Channel is (F - 2402) / 2,

where F is frequency in MHz

[in]| `phy`| Enum [sl_bt_test_phy_t](/bluetooth/<docspace-docleaf-version>/bluetooth-commnd-events-testing-commands/#ga35a5e3ed16a6fc6186b45b47565759bc). PHY to use. Values:
  • sl_bt_test_phy_1m (0x1): 1M PHY

  • sl_bt_test_phy_2m (0x2): 2M PHY

  • sl_bt_test_phy_125k (0x3): 125k Coded PHY

  • sl_bt_test_phy_500k (0x4): 500k Coded PHY

Parameters

  [in]| `power_level`|

TX power level in unit dBm. Values:

  • -127 to +20: Use specified or the nearest TX power level. The minimum -127 dBm is specified in the Bluetooth specification. However, a device may not support this low TX power. In addition, only some devices support 20 dBm TX power.

  • 0x7E: Use minimum TX power level the device supports.

  • 0x7F: Use the smallest of the maximum TX power level the device supports and the global maximum TX power setting in stack.

For continious unmodulated carrier mode, the values are set in deci-dBm values. In case, if the value exceeds the range of power level value, allowed by the device, the command will adjust the power level to the closest minimum or maximum value.

Returns

SL_STATUS_OK if successful. Error code otherwise.

Events

◆ sl_bt_test_dtm_rx()#

sl_status_t sl_bt_test_dtm_rx

(
	 uint8_t 	 channel,
	 uint8_t 	 phy
)

Start a receiver test against a separate Bluetooth tester device. When the command is processed by the radio, a sl_bt_evt_test_dtm_completed event is triggered. This event indicates whether the test started successfully.

Parameter phy specifies which PHY is used to receive the packets. All devices support at least 1M PHY.

The test may be stopped using sl_bt_test_dtm_end command. This will trigger another sl_bt_evt_test_dtm_completed event, which carries the number of packets received during the test.

Parameters

 [in]| `channel`|

Bluetooth channel

Range: 0-39

Channel is (F - 2402) / 2,

where F is frequency in MHz

[in]| `phy`| Enum [sl_bt_test_phy_t](/bluetooth/<docspace-docleaf-version>/bluetooth-commnd-events-testing-commands/#ga35a5e3ed16a6fc6186b45b47565759bc). PHY to use. Values:
  • sl_bt_test_phy_1m (0x1): 1M PHY

  • sl_bt_test_phy_2m (0x2): 2M PHY

  • sl_bt_test_phy_125k (0x3): 125k Coded PHY

  • sl_bt_test_phy_500k (0x4): 500k Coded PHY

Returns

SL_STATUS_OK if successful. Error code otherwise.

Events

◆ sl_bt_test_dtm_end()#

sl_status_t sl_bt_test_dtm_end

(

``

)

End a transmitter or a receiver test. When the command is processed by the radio and the test has ended, a sl_bt_evt_test_dtm_completed event is triggered.

Returns

SL_STATUS_OK if successful. Error code otherwise.

Events