sl_bt_evt_test_dtm_completedTesting Commands#
Indicates that the radio has processed a test start or end command.
Data Structures#
struct | sl_bt_evt_test_dtm_completed_s | Data structure of the dtm_completed event.
Macros#
define | sl_bt_evt_test_dtm_completed_id 0x000e00a0#
| Identifier of the dtm_completed event.
Detailed Description#
Indicates that the radio has processed a test start or end command.
The result parameter indicates the success of the command.
After the receiver or transmitter test is stopped, the number_of_packets
parameter in this event indicates the number of received or transmitted
packets.
Data Structure Documentation#
◆ sl_bt_evt_test_dtm_completed_s#
struct sl_bt_evt_test_dtm_completed_s#
Data structure of the dtm_completed event.
Data Fields#
uint16_t | result |
Command result
uint16_t | number_of_packets |
Number of packets
Only valid for sl_bt_test_dtm_end command.