Testing Commands#
Testing Commands.
Modules#
sl_bt_evt_test_dtm_completed Indicates that the radio has processed a test start or end command.
Enumerations#
enum | sl_bt_test_packet_type_t { sl_bt_test_pkt_prbs9 = 0x0, sl_bt_test_pkt_11110000 = 0x1, sl_bt_test_pkt_10101010 = 0x2, sl_bt_test_pkt_11111111 = 0x4, sl_bt_test_pkt_00000000 = 0x5, sl_bt_test_pkt_00001111 = 0x6, sl_bt_test_pkt_01010101 = 0x7, sl_bt_test_pkt_pn9 = 0xfd, sl_bt_test_pkt_carrier = 0xfe } | Test packet types supported by the stack.
enum | sl_bt_test_phy_t { sl_bt_test_phy_1m = 0x1, sl_bt_test_phy_2m = 0x2, sl_bt_test_phy_125k = 0x3, sl_bt_test_phy_500k = 0x4 } | Test PHY types.
Functions#
sl_status_t | sl_bt_test_dtm_tx_v4 (uint8_t packet_type, uint8_t length, uint8_t channel, uint8_t phy, int8_t power_level)
sl_status_t | sl_bt_test_dtm_tx_cw (uint8_t packet_type, uint8_t channel, uint8_t phy, int16_t power_level)
sl_status_t | sl_bt_test_dtm_rx (uint8_t channel, uint8_t phy)
sl_status_t | sl_bt_test_dtm_end ()
Detailed Description#
Testing Commands.
Enumeration Type Documentation#
◆ sl_bt_test_packet_type_t#
enum sl_bt_test_packet_type_t#
Test packet types supported by the stack.
Enumerator#
sl_bt_test_pkt_prbs9 |
(0x0) PRBS9 packet payload
sl_bt_test_pkt_11110000 |
(0x1) 11110000 packet payload
sl_bt_test_pkt_10101010 |
(0x2) 10101010 packet payload
sl_bt_test_pkt_11111111 |
(0x4) 11111111 packet payload
sl_bt_test_pkt_00000000 |
(0x5) 00000000 packet payload
sl_bt_test_pkt_00001111 |
(0x6) 00001111 packet payload
sl_bt_test_pkt_01010101 |
(0x7) 01010101 packet payload
sl_bt_test_pkt_pn9 |
(0xfd) PN9 continuously modulated output
sl_bt_test_pkt_carrier |
(0xfe) Unmodulated carrier
◆ sl_bt_test_phy_t#
enum sl_bt_test_phy_t#
Test PHY types.
Enumerator#
sl_bt_test_phy_1m |
(0x1) 1M PHY
sl_bt_test_phy_2m |
(0x2) 2M PHY
sl_bt_test_phy_125k |
(0x3) 125k Coded PHY
sl_bt_test_phy_500k |
(0x4) 500k Coded PHY
Function Documentation#
◆ sl_bt_test_dtm_tx_v4()#
sl_status_t sl_bt_test_dtm_tx_v4 | ( | uint8_t |
|
|---|---|---|---|
uint8_t |
| ||
uint8_t |
| ||
uint8_t |
| ||
int8_t |
| ||
) |
Start a transmitter test against a separate Bluetooth tester device. When the command is processed by the radio, a sl_bt_evt_test_dtm_completed event is triggered. This event indicates whether the test started successfully.
In the transmitter test, the device sends packets continuously with a fixed
interval. The type and length of each packet is set by packet_type and
length parameters. The parameter phy specifies which PHY is used to
transmit the packets. All devices support at least 1M PHY. A special packet
type, test_pkt_carrier , can be used to transmit continuous unmodulated
carrier. The length field is ignored in this mode. As this command has the
limitation within the value of power_level, use of
sl_bt_test_dtm_tx_cw for custom
waves is recommended.
Stop the test using the sl_bt_test_dtm_end command.
Parameters
[in] |
| Enum sl_bt_test_packet_type_t. Packet type to transmit. Values:
|
[in] |
| Packet length in bytes Range: 0-255 |
[in] |
| Bluetooth channel Range: 0-39 Channel is (F - 2402) / 2, where F is frequency in MHz |
[in] |
| Enum sl_bt_test_phy_t. PHY to use. Values:
|
[in] |
| TX power level in unit dBm. Values:
|
Returns
SL_STATUS_OK if successful. Error code otherwise.Events
sl_bt_evt_test_dtm_completed - This event is received when the command is processed.
◆ sl_bt_test_dtm_tx_cw()#
sl_status_t sl_bt_test_dtm_tx_cw | ( | uint8_t |
|
|---|---|---|---|
uint8_t |
| ||
uint8_t |
| ||
int16_t |
| ||
) |
Start a transmitter test for a custom wave. When the command is processed by the radio, a sl_bt_evt_test_dtm_completed event is triggered. This event indicates whether the test started successfully.
In the custom wave transmitter test, the device continuously transmits the
career. The parameter packet_type specifies the packet type. The parameter
phy specifies which PHY is used to transmit the packets. All devices support
at least 1M PHY.
Stop the test using the sl_bt_test_dtm_end command.
Parameters
[in] |
| Enum sl_bt_test_packet_type_t. Packet type to transmit. Values:
|
[in] |
| Bluetooth channel Range: 0-39 Channel is (F - 2402) / 2, where F is frequency in MHz |
[in] |
| Enum sl_bt_test_phy_t. PHY to use. Values:
|
[in] |
| TX power level. Unit: 0.1 dBm. If the value exceeds the range of power level value, allowed by the device, the command will adjust the power level to the closest minimum or maximum value. |
Returns
SL_STATUS_OK if successful. Error code otherwise.Events
sl_bt_evt_test_dtm_completed - This event is received when the command is processed.
◆ sl_bt_test_dtm_rx()#
sl_status_t sl_bt_test_dtm_rx | ( | uint8_t |
|
|---|---|---|---|
uint8_t |
| ||
) |
Start a receiver test against a separate Bluetooth tester device. When the command is processed by the radio, a sl_bt_evt_test_dtm_completed event is triggered. This event indicates whether the test started successfully.
Parameter phy specifies which PHY is used to receive the packets. All
devices support at least 1M PHY.
The test may be stopped using sl_bt_test_dtm_end command. This will trigger another sl_bt_evt_test_dtm_completed event, which carries the number of packets received during the test.
Parameters
[in] |
| Bluetooth channel Range: 0-39 Channel is (F - 2402) / 2, where F is frequency in MHz |
[in] |
| Enum sl_bt_test_phy_t. PHY to use. Values:
|
Returns
SL_STATUS_OK if successful. Error code otherwise.Events
sl_bt_evt_test_dtm_completed - This event is received when the command is processed.
◆ sl_bt_test_dtm_end()#
sl_status_t sl_bt_test_dtm_end | ( | `` | ) |
|---|
End a transmitter or a receiver test. When the command is processed by the radio and the test has ended, a sl_bt_evt_test_dtm_completed event is triggered.
Returns
SL_STATUS_OK if successful. Error code otherwise.Events
sl_bt_evt_test_dtm_completed - Received when the command is processed by the radio and the test has ended.