sl_bt_evt_connection_closedConnection#

Indicates that a connection was either closed or that no connection was established from a high duty cycle directed advertising.

Data Structures

struct  

sl_bt_evt_connection_closed_s

Data structure of the closed event.

Macros

#define  

sl_bt_evt_connection_closed_id   0x010600a0

Identifier of the closed event.

Detailed Description#

Indicates that a connection was either closed or that no connection was established from a high duty cycle directed advertising.


Data Structure Documentation#

◆sl_bt_evt_connection_closed_s#

struct sl_bt_evt_connection_closed_s

Data structure of the closed event.

Data Fields

name

description

uint16_t

reason

Reason of connection close. Error code SL_STATUS_BT_CTRL_ADVERTISING_TIMEOUT indicates that the high duty cycle directed advertising timed out and no connection was established. Ignore the value of connection in this case.

uint8_t

connection

Handle of the closed connection